|
#define | SOT (1) |
| The start of transmission delimiter. More...
|
|
#define | EOT (4) |
| The end of transmission delimiter. More...
|
|
#define | UART_RX_STATE_SOT (1) |
| A UART state that expects a SOT to be received as the next character. More...
|
|
#define | UART_RX_STATE_LENGTH (2) |
| A UART state that expects the length to be received as the next character. More...
|
|
#define | UART_RX_STATE_DATA (3) |
| A UART state that expects the next data character to be received. More...
|
|
#define | UART_RX_STATE_EOT (4) |
| A UART state that expects a EOT to be received as the next character. More...
|
|
#define | SIO_BUF_COUNT (3) |
|
#define | SIO_RX_BUF_SIZE (32) |
|
#define | SIO_TX_BUF_SIZE (156) |
|
static uint8_t | sio_rx_buf [SIO_RX_BUF_SIZE] |
| This is the receive buffer of the UART. More...
|
|
static uint8_t | sio_tx_buf [SIO_BUF_COUNT][SIO_TX_BUF_SIZE] |
| This is the transmit buffer of the UART. More...
|
|
static uint8_t * | sio_rx_ptr |
| This pointer points to the next free element inside the receive buffer of the UART. More...
|
|
static uint8_t | sio_rx_state |
| This is the receiver state of the UART. More...
|
|
static uint8_t | sio_rx_length |
| This is the transmit state of the UART. More...
|
|
static uint8_t | data [SIO_RX_BUF_SIZE] |
| This is the buffer to hold the frame received through serial interface. More...
|
|
static uint8_t | data_length = 0 |
| This is length variable to keep track of no of received bytes. More...
|
|
static uint8_t | rx_index = 0 |
| This is index used to validate the received bytes based on their position. More...
|
|
static uint8_t | head = 0 |
| This is head of the queue of buffers to be transmitted. More...
|
|
static uint8_t | buf_count = 0 |
| This is buffer count to keep track of the available bufer for transmission. More...
|
|
bool | remote_cmd_rcvd = false |
| This flag is used to check if a remote_test command has been received or not. More...
|
|
static uint8_t | curr_tx_buffer_index = 0 |
|
static void | process_incoming_sio_data (void) |
| Process data received from SIO. More...
|
|
static uint8_t * | get_next_tx_buffer (void) |
| get the new buffer for next transmission through serial More...
|
|
static void | handle_incoming_msg (void) |
| Parses the Received Data in the Buffer and Process the Commands accordingly. More...
|
|
void | init_sio (void) |
| This function does the initialization of the Serial handler state Machine. More...
|
|
void | serial_data_handler (void) |
| Function to handle the state machine serial data exchange. More...
|
|
void | convert_ota_serial_frame_rx (uint8_t *buf, uint8_t len) |
|
More...
|
|
void | usr_perf_start_confirm (uint8_t status, uint8_t start_mode, trx_config_params_t *trx_config_params, uint8_t peer_ic_type, char *peer_soc_mcu_name, char *peer_trx_name, char *peer_board_name, uint64_t peer_mac_address, float peer_fw_version, uint32_t peer_feature_mask) |
| Function to generate Perf Start confirmation frame that must be sent to host application via serial interface. More...
|
|
void | usr_per_test_start_confirm (uint8_t status) |
| Function to generate Per Test Start confirmation frame that must be sent to host application via serial interface. More...
|
|
void | usr_range_test_beacon_tx (uint8_t *frame) |
| Function to send the transmitted frame to the Host application. More...
|
|
void | usr_range_test_beacon_rsp (uint8_t *mpdu, uint8_t lqi_h, int8_t ed_h, uint8_t lqi_r, int8_t ed_r) |
| Function to send the Received Range Test Response frame to the Host application. More...
|
|
void | usr_range_test_marker_ind (uint8_t *mpdu, uint8_t lqi, int8_t ed_value) |
| Function to send the Marker Indication frame to the Host application. More...
|
|
void | usr_range_test_start_confirm (uint8_t status) |
| Function to generate Range Test Start confirmation frame that must be sent to host application via serial interface. More...
|
|
void | convert_ota_serial_frame_tx (uint8_t *buf, uint8_t len) |
| The Received Remote Reply Command is converted into Serial Data and sent to the Host interface. More...
|
|
void | usr_range_test_stop_confirm (uint8_t status) |
| Function to generate Range Test Stop confirmation frame that must be sent to host application via serial interface. More...
|
|
void | usr_perf_set_confirm (uint8_t status, uint8_t param_type, param_value_t *param_value) |
| Function to generate Perf Set confirmation frame that must be sent to host application via serial interface. More...
|
|
void | usr_perf_get_confirm (uint8_t status, uint8_t param_type, param_value_t *parame_value) |
| Function to generate Perf Get confirmation frame that must be sent to host application via serial interface. More...
|
|
void | usr_identify_peer_node_confirm (uint8_t status) |
| Function to generate Identify_peer_cnode_confirm that must be sent to host application via serial interface. More...
|
|
void | usr_cont_pulse_tx_confirm (uint8_t status) |
| Function to generate cont_pulse_tx_confirm that must be sent to host application via serial interface. More...
|
|
void | usr_cont_wave_tx_confirm (uint8_t status, bool start_stop_param, uint8_t tx_mode) |
| Function to generate cont_wave_tx_confirm that must be sent to host application via serial interface. More...
|
|
void | usr_register_read_confirm (uint8_t status, uint16_t reg_addr, uint8_t reg_val) |
| Function to generate usr_register_read_confirm that must be sent to host application via serial interface. More...
|
|
void | usr_register_write_confirm (uint8_t status, uint16_t reg_addr, uint8_t reg_val) |
| Function to generate usr_register_write_confirm that must be sent to host application via serial interface. More...
|
|
void | usr_register_dump_confirm (uint8_t status, uint16_t start_reg_addr, uint16_t end_reg_addr, uint8_t *reg_val) |
| Function to generate usr_register_dump_confirm that must be sent to host application via serial interface. More...
|
|
void | usr_per_test_end_indication (uint8_t status, int8_t rssi_val, uint8_t aver_lqi, uint32_t frames_transmitted, uint32_t frames_received, uint32_t frames_failure, uint32_t frames_no_ack, uint32_t frames_channel_access_failure, uint32_t frames_with_wrong_crc, float test_duration_sec, float test_net_data_rate) |
| Function to generate Per test End Indication frame that must be sent to host application via serial interface. More...
|
|
void | usr_ed_scan_start_confirm (uint8_t status, uint8_t scan_time_min, float scan_time_sec) |
| Function to generate ED scan confirm test End Indication frame that must be sent to host application via serial interface. More...
|
|
void | usr_pkt_stream_confirm (uint8_t status, bool start_stop) |
|
void | usr_rx_on_confirm (uint8_t status, bool start_stop) |
|
void | usr_ed_scan_end_indication (uint8_t no_of_channels, ed_scan_result_t *ed_scan_result) |
| Function to generate ED scan Indication frame that must be sent to host application via serial interface. More...
|
|
void | usr_sensor_data_get_confirm (uint8_t status, float bat_voltage, float temperature) |
| Function to generate Sensor data confirm frame that must be sent to host application via serial interface. More...
|
|
void | usr_peer_disconnect_confirm (uint8_t status) |
| Function to generate Disconnect Confirm frame that must be sent to host application via serial interface. More...
|
|
void | usr_set_default_config_confirm (uint8_t status, trx_config_params_t *default_trx_config_params) |
| Function to generate Set default config Confirm frame that must be sent to host application via serial interface. More...
|
|
void | usr_identify_board_confirm (uint8_t status, uint8_t ic_type, const char *mcu_soc_name, const char *trx_name, const char *board_name, uint64_t mac_address, float fw_version, uint32_t fw_feature_mask) |
| Function to generate Identify Board confirm frame that must be sent to host application via serial interface. More...
|
|
void | usr_get_current_config_confirm (uint8_t status, trx_config_params_t *curr_trx_conf_params) |
| Function to generate Get Current config Confirm frame that must be sent to host application via serial interface. More...
|
|