|
#define | taskDISABLE_INTERRUPTS() portDISABLE_INTERRUPTS() |
|
#define | taskENABLE_INTERRUPTS() portENABLE_INTERRUPTS() |
|
#define | taskENTER_CRITICAL() portENTER_CRITICAL() |
|
#define | taskEXIT_CRITICAL() portEXIT_CRITICAL() |
|
#define | taskSCHEDULER_NOT_STARTED 0 |
|
#define | taskSCHEDULER_RUNNING 1 |
|
#define | taskSCHEDULER_SUSPENDED 2 |
|
#define | taskYIELD() portYIELD() |
|
#define | tskIDLE_PRIORITY ( ( unsigned portBASE_TYPE ) 0U ) |
|
#define | tskKERNEL_VERSION_NUMBER "V7.3.0" |
|
#define | xTaskCreate(pvTaskCode, pcName, usStackDepth, pvParameters, uxPriority, pxCreatedTask) xTaskGenericCreate( ( pvTaskCode ), ( pcName ), ( usStackDepth ), ( pvParameters ), ( uxPriority ), ( pxCreatedTask ), ( NULL ), ( NULL ) ) |
|
#define | xTaskCreateRestricted(x, pxCreatedTask) xTaskGenericCreate( ((x)->pvTaskCode), ((x)->pcName), ((x)->usStackDepth), ((x)->pvParameters), ((x)->uxPriority), (pxCreatedTask), ((x)->puxStackBuffer), ((x)->xRegions) ) |
|
|
eTaskState | eTaskStateGet (xTaskHandle pxTask) PRIVILEGED_FUNCTION |
| task. More...
|
|
signed char * | pcTaskGetTaskName (xTaskHandle xTaskToQuery) |
|
unsigned portBASE_TYPE | uxTaskGetNumberOfTasks (void) PRIVILEGED_FUNCTION |
|
unsigned portBASE_TYPE | uxTaskGetStackHighWaterMark (xTaskHandle xTask) PRIVILEGED_FUNCTION |
| task.h More...
|
|
unsigned portBASE_TYPE | uxTaskGetTaskNumber (xTaskHandle xTask) |
|
unsigned portBASE_TYPE | uxTaskPriorityGet (xTaskHandle pxTask) PRIVILEGED_FUNCTION |
|
void | vTaskAllocateMPURegions (xTaskHandle xTask, const xMemoryRegion *const pxRegions) PRIVILEGED_FUNCTION |
|
void | vTaskDelay (portTickType xTicksToDelay) PRIVILEGED_FUNCTION |
|
void | vTaskDelayUntil (portTickType *const pxPreviousWakeTime, portTickType xTimeIncrement) PRIVILEGED_FUNCTION |
|
void | vTaskDelete (xTaskHandle pxTaskToDelete) PRIVILEGED_FUNCTION |
|
void | vTaskEndScheduler (void) PRIVILEGED_FUNCTION |
|
void | vTaskGetRunTimeStats (signed char *pcWriteBuffer) PRIVILEGED_FUNCTION |
|
void | vTaskIncrementTick (void) PRIVILEGED_FUNCTION |
|
void | vTaskList (signed char *pcWriteBuffer) PRIVILEGED_FUNCTION |
|
void | vTaskMissedYield (void) PRIVILEGED_FUNCTION |
|
void | vTaskPlaceOnEventList (const xList *const pxEventList, portTickType xTicksToWait) PRIVILEGED_FUNCTION |
|
void | vTaskPlaceOnEventListRestricted (const xList *const pxEventList, portTickType xTicksToWait) PRIVILEGED_FUNCTION |
|
void | vTaskPriorityDisinherit (xTaskHandle *const pxMutexHolder) PRIVILEGED_FUNCTION |
|
void | vTaskPriorityInherit (xTaskHandle *const pxMutexHolder) PRIVILEGED_FUNCTION |
|
void | vTaskPrioritySet (xTaskHandle pxTask, unsigned portBASE_TYPE uxNewPriority) PRIVILEGED_FUNCTION |
|
void | vTaskResume (xTaskHandle pxTaskToResume) PRIVILEGED_FUNCTION |
|
void | vTaskSetTaskNumber (xTaskHandle xTask, unsigned portBASE_TYPE uxHandle) |
|
void | vTaskSetTimeOutState (xTimeOutType *const pxTimeOut) PRIVILEGED_FUNCTION |
|
void | vTaskStartScheduler (void) PRIVILEGED_FUNCTION |
|
void | vTaskStepTick (portTickType xTicksToJump) |
|
void | vTaskSuspend (xTaskHandle pxTaskToSuspend) PRIVILEGED_FUNCTION |
|
void | vTaskSuspendAll (void) PRIVILEGED_FUNCTION |
|
void | vTaskSwitchContext (void) PRIVILEGED_FUNCTION |
|
portBASE_TYPE | xTaskCallApplicationTaskHook (xTaskHandle xTask, void *pvParameter) PRIVILEGED_FUNCTION |
| task.h More...
|
|
portBASE_TYPE | xTaskCheckForTimeOut (xTimeOutType *const pxTimeOut, portTickType *const pxTicksToWait) PRIVILEGED_FUNCTION |
|
signed portBASE_TYPE | xTaskGenericCreate (pdTASK_CODE pxTaskCode, const signed char *const pcName, unsigned short usStackDepth, void *pvParameters, unsigned portBASE_TYPE uxPriority, xTaskHandle *pxCreatedTask, portSTACK_TYPE *puxStackBuffer, const xMemoryRegion *const xRegions) PRIVILEGED_FUNCTION |
|
xTaskHandle | xTaskGetCurrentTaskHandle (void) PRIVILEGED_FUNCTION |
|
xTaskHandle | xTaskGetIdleTaskHandle (void) |
| xTaskGetIdleTaskHandle() is only available if INCLUDE_xTaskGetIdleTaskHandle is set to 1 in FreeRTOSConfig.h. More...
|
|
portBASE_TYPE | xTaskGetSchedulerState (void) PRIVILEGED_FUNCTION |
|
portTickType | xTaskGetTickCount (void) PRIVILEGED_FUNCTION |
|
portTickType | xTaskGetTickCountFromISR (void) PRIVILEGED_FUNCTION |
|
signed portBASE_TYPE | xTaskIsTaskSuspended (xTaskHandle xTask) PRIVILEGED_FUNCTION |
| task. More...
|
|
signed portBASE_TYPE | xTaskRemoveFromEventList (const xList *const pxEventList) PRIVILEGED_FUNCTION |
|
signed portBASE_TYPE | xTaskResumeAll (void) PRIVILEGED_FUNCTION |
|
portBASE_TYPE | xTaskResumeFromISR (xTaskHandle pxTaskToResume) PRIVILEGED_FUNCTION |
|
unsigned portBASE_TYPE uxTaskGetStackHighWaterMark |
( |
xTaskHandle |
xTask | ) |
|
task.h
unsigned portBASE_TYPE uxTaskGetStackHighWaterMark( xTaskHandle xTask );
INCLUDE_uxTaskGetStackHighWaterMark must be set to 1 in FreeRTOSConfig.h for this function to be available.
Returns the high water mark of the stack associated with xTask. That is, the minimum free stack space there has been (in words, so on a 32 bit machine a value of 1 means 4 bytes) since the task started. The smaller the returned number the closer the task has come to overflowing its stack.
- Parameters
-
xTask | Handle of the task associated with the stack to be checked. Set xTask to NULL to check the stack of the calling task. |
- Returns
- The smallest amount of free stack space there has been (in bytes) since the task referenced by xTask was created.