#include "lwip/opt.h"
#include "lwip/pbuf.h"
#include "lwip/ip_addr.h"
#include "lwip/netif.h"
#include "lwip/ip.h"
Data Structures | |
struct | eth_addr |
struct | eth_hdr |
Ethernet header. More... | |
struct | etharp_hdr |
the ARP message, see RFC 826 ("Packet format") More... | |
Macros | |
#define | ARP_REPLY 2 |
#define | ARP_REQUEST 1 |
ARP message types (opcodes) More... | |
#define | ARP_TMR_INTERVAL 5000 |
5 seconds period More... | |
#define | eth_addr_cmp(addr1, addr2) (memcmp((addr1)->addr, (addr2)->addr, ETHARP_HWADDR_LEN) == 0) |
#define | ETHADDR16_COPY(src, dst) SMEMCPY(src, dst, ETHARP_HWADDR_LEN) |
MEMCPY-like macro to copy to/from struct eth_addr's that are no local variables and known to be 16-bit aligned within the protocol header. More... | |
#define | ETHADDR32_COPY(src, dst) SMEMCPY(src, dst, ETHARP_HWADDR_LEN) |
MEMCPY-like macro to copy to/from struct eth_addr's that are local variables or known to be 32-bit aligned within the protocol header. More... | |
#define | etharp_gratuitous(netif) etharp_request((netif), &(netif)->ip_addr) |
For Ethernet network interfaces, we might want to send "gratuitous ARP"; this is an ARP packet sent by a node in order to spontaneously cause other nodes to update an entry in their ARP cache. More... | |
#define | ETHARP_HWADDR_LEN 6 |
#define | etharp_init() /* Compatibility define, not init needed. */ |
#define | ETHTYPE_ARP 0x0806U |
#define | ETHTYPE_IP 0x0800U |
#define | ETHTYPE_PPPOE 0x8864U /* PPP Over Ethernet Session Stage */ |
#define | ETHTYPE_PPPOEDISC 0x8863U /* PPP Over Ethernet Discovery Stage */ |
#define | ETHTYPE_VLAN 0x8100U |
#define | LWIP_ARP_FILTER_NETIF 0 |
Define this to 1 and define LWIP_ARP_FILTER_NETIF_FN(pbuf, netif, type) to a filter function that returns the correct netif when using multiple netifs on one hardware interface where the netif's low-level receive routine cannot decide for the correct netif (e.g. More... | |
#define | SIZEOF_ETH_HDR (14 + ETH_PAD_SIZE) |
#define | SIZEOF_ETHARP_HDR 28 |
#define | SIZEOF_ETHARP_PACKET (SIZEOF_ETH_HDR + SIZEOF_ETHARP_HDR) |
Functions | |
void | etharp_cleanup_netif (struct netif *netif) |
Remove all ARP table entries of the specified netif. More... | |
s8_t | etharp_find_addr (struct netif *netif, ip_addr_t *ipaddr, struct eth_addr **eth_ret, ip_addr_t **ip_ret) |
Finds (stable) ethernet/IP address pair from ARP table using interface and IP address index. More... | |
err_t | etharp_output (struct netif *netif, struct pbuf *q, ip_addr_t *ipaddr) |
Resolve and fill-in Ethernet address header for outgoing IP packet. More... | |
err_t | etharp_query (struct netif *netif, ip_addr_t *ipaddr, struct pbuf *q) |
Send an ARP request for the given IP address and/or queue a packet. More... | |
err_t | etharp_request (struct netif *netif, ip_addr_t *ipaddr) |
Send an ARP request packet asking for ipaddr. More... | |
void | etharp_tmr (void) |
Clears expired entries in the ARP table. More... | |
err_t | ethernet_input (struct pbuf *p, struct netif *netif) |
Process received ethernet frames. More... | |
Variables | |
struct eth_addr ethbroadcast | ethzero |
PACK_STRUCT_BEGIN struct eth_addr | PACK_STRUCT_STRUCT |
#define ARP_REPLY 2 |
Referenced by etharp_arp_input().
#define ARP_REQUEST 1 |
ARP message types (opcodes)
Referenced by etharp_arp_input(), and etharp_request().
#define ARP_TMR_INTERVAL 5000 |
5 seconds period
Referenced by arp_timer(), and sys_timeouts_init().
#define eth_addr_cmp | ( | addr1, | |
addr2 | |||
) | (memcmp((addr1)->addr, (addr2)->addr, ETHARP_HWADDR_LEN) == 0) |
Referenced by ethernet_input().
#define ETHADDR16_COPY | ( | src, | |
dst | |||
) | SMEMCPY(src, dst, ETHARP_HWADDR_LEN) |
MEMCPY-like macro to copy to/from struct eth_addr's that are no local variables and known to be 16-bit aligned within the protocol header.
Referenced by etharp_arp_input(), etharp_raw(), and etharp_send_ip().
#define ETHADDR32_COPY | ( | src, | |
dst | |||
) | SMEMCPY(src, dst, ETHARP_HWADDR_LEN) |
MEMCPY-like macro to copy to/from struct eth_addr's that are local variables or known to be 32-bit aligned within the protocol header.
Referenced by etharp_send_ip(), and etharp_update_arp_entry().
#define etharp_gratuitous | ( | netif | ) | etharp_request((netif), &(netif)->ip_addr) |
For Ethernet network interfaces, we might want to send "gratuitous ARP"; this is an ARP packet sent by a node in order to spontaneously cause other nodes to update an entry in their ARP cache.
From RFC 3220 "IP Mobility Support for IPv4" section 4.6.
Referenced by netif_set_link_up(), and netif_set_up().
#define ETHARP_HWADDR_LEN 6 |
Referenced by etharp_arp_input(), etharp_raw(), etharp_send_ip(), and etharp_update_arp_entry().
#define etharp_init | ( | ) | /* Compatibility define, not init needed. */ |
Referenced by lwip_init().
#define ETHTYPE_ARP 0x0806U |
Referenced by etharp_raw(), ethernet_input(), and ethernetif_input().
#define ETHTYPE_IP 0x0800U |
Referenced by etharp_arp_input(), etharp_raw(), etharp_send_ip(), ethernet_input(), and ethernetif_input().
#define ETHTYPE_PPPOE 0x8864U /* PPP Over Ethernet Session Stage */ |
Referenced by ethernet_input(), and ethernetif_input().
#define ETHTYPE_PPPOEDISC 0x8863U /* PPP Over Ethernet Discovery Stage */ |
Referenced by ethernet_input(), and ethernetif_input().
#define ETHTYPE_VLAN 0x8100U |
Referenced by etharp_arp_input(), and ethernet_input().
#define LWIP_ARP_FILTER_NETIF 0 |
Define this to 1 and define LWIP_ARP_FILTER_NETIF_FN(pbuf, netif, type) to a filter function that returns the correct netif when using multiple netifs on one hardware interface where the netif's low-level receive routine cannot decide for the correct netif (e.g.
when mapping multiple IP addresses to one hardware interface).
#define SIZEOF_ETH_HDR (14 + ETH_PAD_SIZE) |
Referenced by etharp_arp_input(), etharp_raw(), and ethernet_input().
#define SIZEOF_ETHARP_HDR 28 |
#define SIZEOF_ETHARP_PACKET (SIZEOF_ETH_HDR + SIZEOF_ETHARP_HDR) |
Referenced by etharp_arp_input(), and etharp_raw().
Remove all ARP table entries of the specified netif.
netif | points to a network interface |
References arp_table, etharp_free_entry(), ETHARP_STATE_EMPTY, etharp_entry::state, and netif::state.
Referenced by netif_set_down().
s8_t etharp_find_addr | ( | struct netif * | netif, |
ip_addr_t * | ipaddr, | ||
struct eth_addr ** | eth_ret, | ||
ip_addr_t ** | ip_ret | ||
) |
Finds (stable) ethernet/IP address pair from ARP table using interface and IP address index.
netif | points to interface index |
ipaddr | points to the (network order) IP address index |
eth_ret | points to return pointer |
ip_ret | points to return pointer |
References arp_table, etharp_entry::ethaddr, etharp_find_entry(), ETHARP_FLAG_FIND_ONLY, ETHARP_STATE_STABLE, etharp_entry::ipaddr, LWIP_ASSERT, LWIP_UNUSED_ARG, NULL, and netif::state.
Resolve and fill-in Ethernet address header for outgoing IP packet.
For IP multicast and broadcast, corresponding Ethernet addresses are selected and the packet is transmitted on the link.
For unicast addresses, the packet is submitted to etharp_query(). In case the IP address is outside the local network, the IP address of the gateway is used.
netif | The lwIP network interface which the IP packet will be sent on. |
q | The pbuf(s) containing the IP packet to be sent. |
ipaddr | The IP address of the packet destination. |
References arp_table, ERR_BUF, ERR_RTE, etharp_cached_entry, ETHARP_DEBUG, etharp_output_to_arp_index(), etharp_query(), etharp_send_ip(), ETHARP_SET_HINT, ETHARP_STATE_STABLE, ETHARP_STATS_INC, netif::gw, netif::hwaddr, ip4_addr2, ip4_addr3, ip4_addr4, netif::ip_addr, ip_addr_cmp, ip_addr_isany, ip_addr_isbroadcast, ip_addr_islinklocal, ip_addr_ismulticast, ip_addr_netcmp, LINK_STATS_INC, LL_MULTICAST_ADDR_0, LL_MULTICAST_ADDR_1, LL_MULTICAST_ADDR_2, LWIP_ASSERT, LWIP_DBG_LEVEL_SERIOUS, LWIP_DBG_TRACE, LWIP_DEBUGF, netif::netmask, NULL, pbuf::payload, and pbuf_header().
Referenced by ethernetif_init().
Send an ARP request for the given IP address and/or queue a packet.
If the IP address was not yet in the cache, a pending ARP cache entry is added and an ARP request is sent for the given address. The packet is queued on this entry.
If the IP address was already pending in the cache, a new ARP request is sent for the given address. The packet is queued on this entry.
If the IP address was already stable in the cache, and a packet is given, it is directly sent and no ARP request is sent out.
If the IP address was already stable in the cache, and no packet is given, an ARP request is sent out.
netif | The lwIP network interface on which ipaddr must be queried for. |
ipaddr | The IP address to be resolved. |
q | If non-NULL, a pbuf that must be delivered to the IP address. q is not freed by this function. |
References arp_table, ERR_ARG, ERR_MEM, ERR_OK, ETHARP_DEBUG, etharp_find_entry(), ETHARP_FLAG_TRY_HARD, etharp_request(), etharp_send_ip(), ETHARP_SET_HINT, ETHARP_STATE_EMPTY, ETHARP_STATE_PENDING, ETHARP_STATE_STABLE, ETHARP_STATS_INC, netif::hwaddr, if(), ip_addr_isany, ip_addr_isbroadcast, ip_addr_ismulticast, pbuf::len, LWIP_ASSERT, LWIP_DBG_TRACE, LWIP_DEBUGF, memp_malloc(), pbuf::next, NULL, pbuf_alloc(), pbuf_copy(), pbuf_free(), PBUF_RAM, PBUF_RAW, pbuf_ref(), PBUF_ROM, etharp_entry::q, S16_F, etharp_entry::state, pbuf::tot_len, and pbuf::type.
Referenced by dhcp_check(), and etharp_output().
Send an ARP request packet asking for ipaddr.
netif | the lwip network interface on which to send the request |
ipaddr | the IP address for which to ask |
References ARP_REQUEST, ETHARP_DEBUG, etharp_raw(), netif::hwaddr, netif::ip_addr, LWIP_DBG_TRACE, and LWIP_DEBUGF.
Referenced by etharp_output_to_arp_index(), and etharp_query().
Clears expired entries in the ARP table.
This function should be called every ETHARP_TMR_INTERVAL milliseconds (5 seconds), in order to expire entries in the ARP table.
References ARP_MAXAGE, ARP_MAXPENDING, arp_table, etharp_entry::ctime, ETHARP_DEBUG, etharp_free_entry(), ETHARP_STATE_EMPTY, ETHARP_STATE_PENDING, ETHARP_STATE_STABLE, ETHARP_STATE_STABLE_REREQUESTING, LWIP_DEBUGF, etharp_entry::state, and U16_F.
Referenced by arp_timer().
Process received ethernet frames.
Using this function instead of directly calling ip_input and passing ARP frames through etharp in ethernetif_input, the ARP cache is protected from concurrent access.
p | the recevied packet, p->payload pointing to the ethernet header |
netif | the network interface on which the packet was received |
References ERR_OK, eth_addr_cmp, etharp_arp_input(), ETHARP_DEBUG, ETHARP_STATS_INC, ETHTYPE_ARP, ETHTYPE_IP, ETHTYPE_PPPOE, ETHTYPE_PPPOEDISC, ETHTYPE_VLAN, pbuf::flags, netif::flags, htons, netif::hwaddr, ip_input(), pbuf::len, LL_MULTICAST_ADDR_0, LL_MULTICAST_ADDR_1, LL_MULTICAST_ADDR_2, LWIP_ASSERT, LWIP_DBG_TRACE, LWIP_DEBUGF, NETIF_FLAG_ETHARP, pbuf::payload, PBUF_FLAG_LLBCAST, PBUF_FLAG_LLMCAST, pbuf_free(), pbuf_header(), PP_HTONS, SIZEOF_ETH_HDR, and X8_F.
Referenced by tcpip_input(), and tcpip_thread().
struct eth_addr ethbroadcast ethzero |
Referenced by etharp_free_entry().
PACK_STRUCT_BEGIN struct etharp_hdr PACK_STRUCT_STRUCT |