#include "lwip/opt.h"
#include "lwip/def.h"
#include "lwip/pbuf.h"
#include "lwip/ip_addr.h"
#include "lwip/err.h"
#include "lwip/netif.h"
Data Structures | |
struct | ip_hdr |
struct | ip_pcb |
Macros | |
#define | ip_current_dest_addr() (¤t_iphdr_dest) |
Destination IP address of current_header. More... | |
#define | ip_current_header() (current_header) |
Get the IP header of the current packet. More... | |
#define | ip_current_netif() (current_netif) |
Get the interface that received the current packet. More... | |
#define | ip_current_src_addr() (¤t_iphdr_src) |
Source IP address of current_header. More... | |
#define | ip_debug_print(p) |
#define | IP_DF 0x4000U /* dont fragment flag */ |
#define | ip_get_option(pcb, opt) ((pcb)->so_options & (opt)) |
Gets an IP pcb option (SOF_* flags) More... | |
#define | IP_HDRINCL NULL |
#define | IP_HLEN 20 |
#define | ip_init() /* Compatibility define, not init needed. */ |
#define | IP_MF 0x2000U /* more fragments flag */ |
#define | IP_OFFMASK 0x1fffU /* mask for fragmenting bits */ |
#define | IP_OPTIONS_SEND LWIP_IGMP |
Currently, the function ip_output_if_opt() is only used with IGMP. More... | |
#define | IP_PCB |
#define | IP_PCB_ADDRHINT |
#define | IP_PROTO_ICMP 1 |
#define | IP_PROTO_IGMP 2 |
#define | IP_PROTO_TCP 6 |
#define | IP_PROTO_UDP 17 |
#define | IP_PROTO_UDPLITE 136 |
#define | ip_reset_option(pcb, opt) ((pcb)->so_options &= ~(opt)) |
Resets an IP pcb option (SOF_* flags) More... | |
#define | IP_RF 0x8000U /* reserved fragment flag */ |
#define | ip_set_option(pcb, opt) ((pcb)->so_options |= (opt)) |
Sets an IP pcb option (SOF_* flags) More... | |
#define | IPH_CHKSUM(hdr) ((hdr)->_chksum) |
#define | IPH_CHKSUM_SET(hdr, chksum) (hdr)->_chksum = (chksum) |
#define | IPH_HL(hdr) ((hdr)->_v_hl & 0x0f) |
#define | IPH_ID(hdr) ((hdr)->_id) |
#define | IPH_ID_SET(hdr, id) (hdr)->_id = (id) |
#define | IPH_LEN(hdr) ((hdr)->_len) |
#define | IPH_LEN_SET(hdr, len) (hdr)->_len = (len) |
#define | IPH_OFFSET(hdr) ((hdr)->_offset) |
#define | IPH_OFFSET_SET(hdr, off) (hdr)->_offset = (off) |
#define | IPH_PROTO(hdr) ((hdr)->_proto) |
#define | IPH_PROTO_SET(hdr, proto) (hdr)->_proto = (u8_t)(proto) |
#define | IPH_TOS(hdr) ((hdr)->_tos) |
#define | IPH_TOS_SET(hdr, tos) (hdr)->_tos = (tos) |
#define | IPH_TTL(hdr) ((hdr)->_ttl) |
#define | IPH_TTL_SET(hdr, ttl) (hdr)->_ttl = (u8_t)(ttl) |
#define | IPH_V(hdr) ((hdr)->_v_hl >> 4) |
#define | IPH_VHL_SET(hdr, v, hl) (hdr)->_v_hl = (((v) << 4) | (hl)) |
#define | SOF_ACCEPTCONN 0x02U /* socket has had listen() */ |
#define | SOF_BROADCAST 0x20U /* permit to send and to receive broadcast messages (see IP_SOF_BROADCAST option) */ |
#define | SOF_INHERITED (SOF_REUSEADDR|SOF_KEEPALIVE|SOF_LINGER/*|SOF_DEBUG|SOF_DONTROUTE|SOF_OOBINLINE*/) |
#define | SOF_KEEPALIVE 0x08U /* keep connections alive */ |
#define | SOF_LINGER 0x80U /* linger on close if data present */ |
#define | SOF_REUSEADDR 0x04U /* allow local address reuse */ |
Functions | |
err_t | ip_input (struct pbuf *p, struct netif *inp) |
This function is called by the network interface device driver when an IP packet is received. More... | |
err_t | ip_output (struct pbuf *p, ip_addr_t *src, ip_addr_t *dest, u8_t ttl, u8_t tos, u8_t proto) |
Simple interface to ip_output_if. More... | |
err_t | ip_output_if (struct pbuf *p, ip_addr_t *src, ip_addr_t *dest, u8_t ttl, u8_t tos, u8_t proto, struct netif *netif) |
Sends an IP packet on a network interface. More... | |
struct netif * | ip_route (ip_addr_t *dest) |
Finds the appropriate network interface for a given IP address. More... | |
Variables | |
struct ip_hdr * | current_header |
Header of the input packet currently being processed. More... | |
ip_addr_t | current_iphdr_dest |
Destination IP address of current_header. More... | |
ip_addr_t | current_iphdr_src |
Source IP address of current_header. More... | |
struct netif * | current_netif |
The interface that provided the packet for the current callback invocation. More... | |
PACK_STRUCT_BEGIN struct ip_hdr | PACK_STRUCT_STRUCT |
#define ip_current_dest_addr | ( | ) | (¤t_iphdr_dest) |
Destination IP address of current_header.
Referenced by icmp_input(), recv_udp(), tcp_input(), tcp_listen_input(), tcp_process(), tcp_timewait_input(), and udp_input().
#define ip_current_header | ( | ) | (current_header) |
Get the IP header of the current packet.
This function must only be called from a receive callback (udp_recv, raw_recv, tcp_accept). It will return NULL otherwise.
Referenced by recv_udp().
#define ip_current_netif | ( | ) | (current_netif) |
Get the interface that received the current packet.
This function must only be called from a receive callback (udp_recv, raw_recv, tcp_accept). It will return NULL otherwise.
#define ip_current_src_addr | ( | ) | (¤t_iphdr_src) |
Source IP address of current_header.
Referenced by icmp_input(), tcp_input(), tcp_listen_input(), tcp_process(), tcp_timewait_input(), and udp_input().
#define ip_debug_print | ( | p | ) |
Referenced by ip_input().
#define IP_DF 0x4000U /* dont fragment flag */ |
#define ip_get_option | ( | pcb, | |
opt | |||
) | ((pcb)->so_options & (opt)) |
Gets an IP pcb option (SOF_* flags)
Referenced by tcp_bind(), tcp_connect(), tcp_listen_with_backlog(), tcp_slowtmr(), udp_bind(), and udp_input().
#define IP_HDRINCL NULL |
Referenced by icmp_input().
#define IP_HLEN 20 |
#define ip_init | ( | ) | /* Compatibility define, not init needed. */ |
Referenced by lwip_init().
#define IP_MF 0x2000U /* more fragments flag */ |
Referenced by ip_frag(), ip_input(), and ip_reass().
#define IP_OFFMASK 0x1fffU /* mask for fragmenting bits */ |
Referenced by ip_frag(), ip_input(), ip_reass(), and ip_reass_chain_frag_into_datagram_and_validate().
#define IP_OPTIONS_SEND LWIP_IGMP |
Currently, the function ip_output_if_opt() is only used with IGMP.
#define IP_PCB |
#define IP_PCB_ADDRHINT |
#define IP_PROTO_ICMP 1 |
Referenced by icmp_input(), icmp_send_response(), and ip_input().
#define IP_PROTO_IGMP 2 |
Referenced by ip_input().
#define IP_PROTO_TCP 6 |
Referenced by ip_input(), tcp_input(), tcp_keepalive(), tcp_output_segment(), tcp_rst(), tcp_send_empty_ack(), and tcp_zero_window_probe().
#define IP_PROTO_UDP 17 |
Referenced by ip_input(), and udp_input().
#define IP_PROTO_UDPLITE 136 |
Referenced by ip_input(), and udp_input().
#define ip_reset_option | ( | pcb, | |
opt | |||
) | ((pcb)->so_options &= ~(opt)) |
Resets an IP pcb option (SOF_* flags)
#define IP_RF 0x8000U /* reserved fragment flag */ |
#define ip_set_option | ( | pcb, | |
opt | |||
) | ((pcb)->so_options |= (opt)) |
Sets an IP pcb option (SOF_* flags)
Referenced by dhcp_inform(), dhcp_start(), and tcp_listen_with_backlog().
#define IPH_CHKSUM | ( | hdr | ) | ((hdr)->_chksum) |
#define IPH_CHKSUM_SET | ( | hdr, | |
chksum | |||
) | (hdr)->_chksum = (chksum) |
Referenced by icmp_input(), ip_frag(), and ip_reass().
#define IPH_HL | ( | hdr | ) | ((hdr)->_v_hl & 0x0f) |
Referenced by icmp_input(), ip_input(), ip_reass(), ip_reass_chain_frag_into_datagram_and_validate(), tcp_input(), and udp_input().
#define IPH_ID | ( | hdr | ) | ((hdr)->_id) |
Referenced by ip_input(), and ip_reass().
#define IPH_ID_SET | ( | hdr, | |
id | |||
) | (hdr)->_id = (id) |
#define IPH_LEN | ( | hdr | ) | ((hdr)->_len) |
Referenced by ip_input(), ip_reass(), ip_reass_chain_frag_into_datagram_and_validate(), and recv_udp().
#define IPH_LEN_SET | ( | hdr, | |
len | |||
) | (hdr)->_len = (len) |
Referenced by ip_frag(), and ip_reass().
#define IPH_OFFSET | ( | hdr | ) | ((hdr)->_offset) |
Referenced by ip_frag(), ip_input(), ip_reass(), and ip_reass_chain_frag_into_datagram_and_validate().
#define IPH_OFFSET_SET | ( | hdr, | |
off | |||
) | (hdr)->_offset = (off) |
Referenced by ip_frag(), and ip_reass().
#define IPH_PROTO | ( | hdr | ) | ((hdr)->_proto) |
Referenced by ip_input(), and udp_input().
#define IPH_PROTO_SET | ( | hdr, | |
proto | |||
) | (hdr)->_proto = (u8_t)(proto) |
#define IPH_TOS | ( | hdr | ) | ((hdr)->_tos) |
#define IPH_TOS_SET | ( | hdr, | |
tos | |||
) | (hdr)->_tos = (tos) |
#define IPH_TTL | ( | hdr | ) | ((hdr)->_ttl) |
#define IPH_TTL_SET | ( | hdr, | |
ttl | |||
) | (hdr)->_ttl = (u8_t)(ttl) |
Referenced by icmp_input().
#define IPH_V | ( | hdr | ) | ((hdr)->_v_hl >> 4) |
Referenced by ip_input().
#define IPH_VHL_SET | ( | hdr, | |
v, | |||
hl | |||
) | (hdr)->_v_hl = (((v) << 4) | (hl)) |
#define SOF_ACCEPTCONN 0x02U /* socket has had listen() */ |
Referenced by tcp_listen_with_backlog().
#define SOF_BROADCAST 0x20U /* permit to send and to receive broadcast messages (see IP_SOF_BROADCAST option) */ |
Referenced by dhcp_inform(), dhcp_start(), and udp_input().
#define SOF_INHERITED (SOF_REUSEADDR|SOF_KEEPALIVE|SOF_LINGER/*|SOF_DEBUG|SOF_DONTROUTE|SOF_OOBINLINE*/) |
Referenced by tcp_listen_input().
#define SOF_KEEPALIVE 0x08U /* keep connections alive */ |
Referenced by tcp_slowtmr().
#define SOF_LINGER 0x80U /* linger on close if data present */ |
#define SOF_REUSEADDR 0x04U /* allow local address reuse */ |
Referenced by tcp_bind(), tcp_connect(), tcp_listen_with_backlog(), udp_bind(), and udp_input().
This function is called by the network interface device driver when an IP packet is received.
The function does the basic checks of the IP header such as packet size being at least larger than the header size etc. If the packet was not destined for us, the packet is forwarded (using ip_forward). The IP checksum is always checked.
Finally, the packet is sent to the upper layer protocol input function.
p | the received IP packet (p->payload points to IP header) |
inp | the netif on which this packet was received |
References current_iphdr_dest, current_iphdr_src, ERR_OK, netif::flags, icmp_dest_unreach(), ICMP_DUR_PROTO, icmp_input(), if(), inet_chksum(), ip4_addr_get_u32, IP_ACCEPT_LINK_LAYER_ADDRESSED_PORT, netif::ip_addr, ip_addr_cmp, ip_addr_copy, ip_addr_isany, ip_addr_isbroadcast, ip_addr_ismulticast, ip_addr_set_any, IP_DEBUG, ip_debug_print, IP_HLEN, IP_MF, IP_OFFMASK, IP_PROTO_ICMP, IP_PROTO_IGMP, IP_PROTO_TCP, IP_PROTO_UDP, IP_PROTO_UDPLITE, ip_reass(), IP_STATS_INC, IPH_HL, IPH_ID, IPH_LEN, IPH_OFFSET, IPH_PROTO, IPH_V, iphdr, pbuf::len, LWIP_DBG_LEVEL_SERIOUS, LWIP_DBG_LEVEL_WARNING, LWIP_DBG_TRACE, LWIP_DEBUGF, netif::name, NETIF_FLAG_IGMP, netif_is_up, netif_list, netif::netmask, netif::next, ntohs, NULL, pbuf::payload, pbuf_free(), pbuf_realloc(), PP_HTONS, snmp_inc_ipinaddrerrors, snmp_inc_ipindelivers, snmp_inc_ipindiscards, snmp_inc_ipinhdrerrors, snmp_inc_ipinreceives, snmp_inc_ipinunknownprotos, tcp_input(), pbuf::tot_len, udp_input(), X16_F, and X32_F.
Referenced by ethernet_input(), netif_init(), tcpip_input(), and tcpip_thread().
err_t ip_output | ( | struct pbuf * | p, |
ip_addr_t * | src, | ||
ip_addr_t * | dest, | ||
u8_t | ttl, | ||
u8_t | tos, | ||
u8_t | proto | ||
) |
Simple interface to ip_output_if.
It finds the outgoing network interface and calls upon ip_output_if to do the actual work.
p | the packet to send (p->payload points to the data, e.g. next protocol header; if dest == IP_HDRINCL, p already includes an IP header and p->payload points to that IP header) |
src | the source IP address to send from (if src == IP_ADDR_ANY, the IP address of the netif used to send is used as source address) |
dest | the destination IP address to send the packet to |
ttl | the TTL value to be set in the IP header |
tos | the TOS value to be set in the IP header |
proto | the PROTOCOL to be set in the IP header |
References ERR_RTE, ip4_addr1_16, ip4_addr2_16, ip4_addr3_16, ip4_addr4_16, IP_DEBUG, ip_output_if(), ip_route(), IP_STATS_INC, LWIP_ASSERT, LWIP_DEBUGF, NULL, and pbuf::ref.
Referenced by icmp_send_response(), tcp_keepalive(), tcp_output_segment(), tcp_rst(), tcp_send_empty_ack(), and tcp_zero_window_probe().
err_t ip_output_if | ( | struct pbuf * | p, |
ip_addr_t * | src, | ||
ip_addr_t * | dest, | ||
u8_t | ttl, | ||
u8_t | tos, | ||
u8_t | proto, | ||
struct netif * | netif | ||
) |
Sends an IP packet on a network interface.
This function constructs the IP header and calculates the IP header checksum. If the source IP address is NULL, the IP address of the outgoing network interface is filled in as source address. If the destination IP address is IP_HDRINCL, p is assumed to already include an IP header and p->payload points to it instead of the data.
p | the packet to send (p->payload points to the data, e.g. next protocol header; if dest == IP_HDRINCL, p already includes an IP header and p->payload points to that IP header) |
src | the source IP address to send from (if src == IP_ADDR_ANY, the IP address of the netif used to send is used as source address) |
dest | the destination IP address to send the packet to |
ttl | the TTL value to be set in the IP header |
tos | the TOS value to be set in the IP header |
proto | the PROTOCOL to be set in the IP header |
netif | the netif on which to send this packet |
References NULL.
Referenced by icmp_input(), and ip_output().
Finds the appropriate network interface for a given IP address.
It searches the list of network interfaces linearly. A match is found if the masked IP address of the network interface equals the masked IP address given to the function.
dest | the destination IP address for which to find the route |
References ip4_addr1_16, ip4_addr2_16, ip4_addr3_16, ip4_addr4_16, netif::ip_addr, ip_addr_netcmp, IP_DEBUG, IP_STATS_INC, LWIP_DBG_LEVEL_SERIOUS, LWIP_DEBUGF, netif_default, netif_is_up, netif_list, netif::netmask, netif::next, NULL, snmp_inc_ipoutnoroutes, and U16_F.
Referenced by etharp_update_arp_entry(), ip_output(), tcp_connect(), tcp_eff_send_mss(), tcp_output_segment(), and udp_connect().
struct ip_hdr* current_header |
Header of the input packet currently being processed.
ip_addr_t current_iphdr_dest |
Destination IP address of current_header.
Referenced by icmp_input(), ip_input(), tcp_input(), tcp_listen_input(), and udp_input().
ip_addr_t current_iphdr_src |
Source IP address of current_header.
Referenced by ip_input(), tcp_input(), tcp_listen_input(), and udp_input().
struct netif* current_netif |
The interface that provided the packet for the current callback invocation.
PACK_STRUCT_BEGIN struct ip_hdr PACK_STRUCT_STRUCT |