HTTP component task for the HTTP Netconn Example.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
#include "task_defs.h"
#include "stdio_serial.h"
#include "ethernet.h"
#include "sysclk.h"
#include "lwip/opt.h"
#include "lwip/tcpip.h"
#include "httpd.h"
#include "tc.h"
#include "lwip/stats.h"
Functions | |
static void | configure_timer_for_bandwidth_stats (void) |
Enable TC1 channel 0 to trigger each second to compute GMAC stats. More... | |
void | create_http_task (uint16_t stack_depth_words, unsigned portBASE_TYPE task_priority) |
Create the HTTP task. More... | |
static void | http_task (void *pvParameters) |
HTTP task core function. More... | |
void | TC3_Handler (void) |
Variables | |
uint32_t | lwip_rx_count |
uint32_t | lwip_rx_rate |
uint32_t | lwip_tx_count |
Used to compute LwIP bandwidth. More... | |
uint32_t | lwip_tx_rate |
Enable TC1 channel 0 to trigger each second to compute GMAC stats.
References pmc_enable_periph_clk(), tc_enable_interrupt(), tc_init(), tc_start(), and tc_write_rc().
Referenced by http_task().
void create_http_task | ( | uint16_t | stack_depth_words, |
unsigned portBASE_TYPE | task_priority | ||
) |
Create the HTTP task.
stack_depth_words | Task stack size in 32 bits word. |
task_priority | Task priority. |
References http_task(), NULL, and xTaskCreate.
Referenced by main().
HTTP task core function.
pvParameters | Junk parameter. |
References configure_timer_for_bandwidth_stats(), ERR_OK, http_request(), mainHTTP_TASK_PRIORITY, mainHTTP_TASK_STACK_SIZE, netconn_accept(), netconn_bind(), netconn_close(), netconn_delete(), netconn_listen, netconn_new, NETCONN_TCP, NULL, sys_thread_new(), UNUSED, vTaskDelete(), and WAIT_FOR_TOUCH_EVENT.
Referenced by create_http_task().
References lwip_rx_count, lwip_rx_rate, lwip_tx_count, lwip_tx_rate, and tc_get_status().
uint32_t lwip_rx_count |
Referenced by ksz8851snl_low_level_input(), and TC3_Handler().
uint32_t lwip_rx_rate |
Referenced by cgi_status(), and TC3_Handler().
uint32_t lwip_tx_count |
Used to compute LwIP bandwidth.
Used to compute LwIP bandwidth.
Referenced by ksz8851snl_low_level_output(), and TC3_Handler().
uint32_t lwip_tx_rate |
Referenced by cgi_status(), and TC3_Handler().