Microchip® Advanced Software Framework

qdebug.h File Reference
#include "touch_api.h"

Macros

#define SUBS_SIGN_ON   0
 
#define SUBS_GLOBAL_CONFIG   1
 
#define SUBS_SENSOR_CONFIG   2
 
#define SUBS_SIGNALS   3
 
#define SUBS_REF   4
 
#define SUBS_DELTA   5
 
#define SUBS_STATES   6
 
#define QT_CMD_DUMMY   0x10
 
#define QT_CMD_SET_SUBS   0x11
 
#define QT_CMD_SET_GLOBAL_CONFIG   0x12
 
#define QT_CMD_SET_CH_CONFIG   0x13
 
#define QT_CMD_SET_QM_BURST_LENGTHS   0x14
 
#define QT_CMD_SET_USER_DATA   0x15
 
#define QT_DUMMY   0x20
 
#define QT_SIGN_ON   0x21
 
#define QT_GLOBAL_CONFIG   0x22
 
#define QT_SENSOR_CONFIG   0x23
 
#define QT_SIGNALS   0x24
 
#define QT_REFERENCES   0x25
 
#define QT_DELTAS   0x26
 
#define QT_STATES   0x27
 
#define QT_MESSAGE_START   0x1B
 

Functions

void QDebug_Init (void)
 Initialize Debug InterfaceMust be called before the main loop. More...
 
void QDebug_ProcessCommands (void)
 Command handler for the data received from QTouch StudioThis function should be called in the main loop after measure_sensors to process the data received from QTOuch Studio More...
 
void QDebug_SendData (uint16_t qt_lib_flags)
 Send data to QTouch Studio based on the subscriptionThis function should be called in the main loop after measure_sensors to send the measured touch data. More...
 
void QDebug_SetSubscriptions (uint16_t once, uint16_t change, uint16_t allways)
 Set subscription values. More...
 
int16_t qt_get_sensor_delta (uint8_t)
 
void Set_Channel_Config (void)
 Extract the data packet from QTouch Studio and set channel configShould only be called from the command handler. More...
 
void Set_Global_Config (void)
 Extract the data packet from QTouch Studio and set global configShould only be called from the command handler. More...
 
void Set_Measurement_Period (void)
 
void Set_QM_Burst_Lengths (void)
 Set QMatrix burst lengthsShould only be called from the command handler. More...
 
void Set_QT_User_Data (uint8_t *)
 Extracts user data from QTouch Studio to touch mcu memoryThe data can be binary data. More...
 
void Set_Subscriptions (void)
 Set Data Subscription valuesShould only be called from the command handler. More...
 
void Transmit_Burst_Lengths (void)
 Transmits the QMatrix burst length values to QTouch StudioThis value is available for each channel. More...
 
void Transmit_Delta (void)
 Transmits the channel delta values to QTouch StudioThe value is equal to signal-reference. More...
 
void Transmit_Dummy (void)
 Transmits a dummy packet if no other subscriptions are set. More...
 
void Transmit_Global_Config (void)
 Transmits the global config struct to QTouch Studio. More...
 
void Transmit_QT_User_Data (uint8_t *pdata, uint16_t c)
 Transmits user data to QTouch StudioThe data will be binary data. More...
 
void Transmit_Ref (void)
 Transmits the channel reference values to QTouch Studio. More...
 
void Transmit_Sensor_Config (void)
 Transmits the channel config struct to QTouch Studio. More...
 
void Transmit_Sign_On (void)
 Transmits the sign on packet to QTouch Studio. More...
 
void Transmit_Signals (void)
 Transmits the measurement values for each channel to QTouch Studio. More...
 
void Transmit_State (void)
 Transmits the state values to QTouch StudioOn/Off condition for each sensor. More...
 
void Transmit_Time_Stamps (void)
 Transmits the application execution timestamp values to QTouch StudioThis value is a combination of current_time_ms_touch (high word) & timer counter register (low word) More...
 

Variables

qt_touch_lib_config_data_t qt_config_data
 
qt_touch_lib_measure_data_t qt_measure_data
 

int16_t qt_get_sensor_delta ( uint8_t  )
void Set_Measurement_Period ( void  )
void Transmit_Ref ( void  )

Transmits the channel reference values to QTouch Studio.

References tag_qt_touch_lib_measure_data_t::channel_references, PutChar(), qt_measure_data, QT_NUM_CHANNELS, QT_REFERENCES, and Send_Message().

Referenced by app_task().

qt_touch_lib_measure_data_t qt_measure_data