Macros | |
#define | _QMATRIX_ |
The following rules need to be followed while configuring the QTouch library for QTouch acquisition method. More... | |
#define | _QMATRIX_ |
The following rules need to be followed while configuring the QTouch library for QTouch acquisition method. More... | |
#define | _ROTOR_SLIDER_ |
#define | DEF_QT_DI 4u |
#define | DEF_QT_DRIFT_HOLD_TIME 20 /* 4s */ |
#define | DEF_QT_MAX_ON_DURATION 0 /* disabled */ |
#define | DEF_QT_NEG_DRIFT_RATE 20 /* 4s per LSB */ |
#define | DEF_QT_POS_DRIFT_RATE 5 /* 1s per LSB */ |
#define | DEF_QT_POS_RECAL_DELAY 3u |
#define | DEF_QT_RECAL_THRESHOLD RECAL_50 /* recal threshold = 50% of detect */ |
#define | NUM_X_LINES 5 |
Define the Number X lines to be used. More... | |
#define | NUM_X_PORTS 2 |
Specify the number of ports on which X-lines that are distributed. More... | |
#define | NUM_Y_LINES 4 |
Define the Number Y lines and port for YA, YB to be used. More... | |
#define | PORT_NUM_1 1 |
#define | PORT_NUM_2 2 |
#define | PORT_SMP D |
Specify the port for SMP. More... | |
#define | PORT_SMP D |
Specify the port for SMP. More... | |
#define | PORT_X_1 D |
Specify Which ports have X lines on them. More... | |
#define | PORT_X_2 B |
#define | PORT_YA G |
#define | PORT_YB F |
#define | QT_DELAY_CYCLES 2 |
Example configuration based on option selected in project options. More... | |
#define | QT_DELAY_CYCLES 2 |
Example configuration based on option selected in project options. More... | |
#define | QT_MAX_NUM_ROTORS_SLIDERS 4 |
#define | QT_NUM_CHANNELS 32 |
Number of Channels(dependent on the library used and application requirement). More... | |
#define | SHARED_YAYB 0 |
Specify if YA and YB share the same port. More... | |
#define | SMP_PIN 5 |
#define | SMP_PIN 5 |
#define | TICKS_PER_MS 15u /* (16MHz/1024)* (1/1000) */ |
Total ticks per msec. More... | |
#define _QMATRIX_ |
The following rules need to be followed while configuring the QTouch library for QTouch acquisition method.
#define QT_DELAY_CYCLES
The value for QT_NUM_CHANNELS should match the library chosen. For example, when using libavr5g4-64qm-8x-8y-krs-4rs.a library, set QT_NUM_CHANNELS to 64 only.
#define NUM_X_PORTS
#define PORT_NUM_1
#define PORT_NUM_2 <value, if using 2 X ports> #define PORT_NUM_3 <value, if using 3 X ports> #define PORT_X_1
#define PORT_X_2 <value, if using 2 X ports> #define PORT_X_3 <value, if using 3 X ports>
#define PORT_YA
#define PORT_YB
#define SMP_PIN
The value for QT_MAX_NUM_ROTOR_SLIDER should match the library chosen. For example, when using libavr5g4-64qm-8x-8y-krs-4rs.a library, set QT_MAX_NUM_ROTOR_SLIDER to 4 only.
#define _QMATRIX_ |
The following rules need to be followed while configuring the QTouch library for QTouch acquisition method.
#define QT_DELAY_CYCLES
The value for QT_NUM_CHANNELS should match the library chosen. For example, when using libavr5g4-64qm-8x-8y-krs-4rs.a library, set QT_NUM_CHANNELS to 64 only.
#define NUM_X_PORTS
#define PORT_NUM_1
#define PORT_NUM_2 <value, if using 2 X ports> #define PORT_NUM_3 <value, if using 3 X ports> #define PORT_X_1
#define PORT_X_2 <value, if using 2 X ports> #define PORT_X_3 <value, if using 3 X ports>
#define PORT_YA
#define PORT_YB
#define SMP_PIN
The value for QT_MAX_NUM_ROTOR_SLIDER should match the library chosen. For example, when using libavr5g4-64qm-8x-8y-krs-4rs.a library, set QT_MAX_NUM_ROTOR_SLIDER to 4 only.
#define _ROTOR_SLIDER_ |
#define DEF_QT_DI 4u |
Referenced by qt_set_parameters().
#define DEF_QT_DRIFT_HOLD_TIME 20 /* 4s */ |
Referenced by qt_set_parameters().
#define DEF_QT_MAX_ON_DURATION 0 /* disabled */ |
Referenced by qt_set_parameters().
#define DEF_QT_NEG_DRIFT_RATE 20 /* 4s per LSB */ |
Referenced by qt_set_parameters().
#define DEF_QT_POS_DRIFT_RATE 5 /* 1s per LSB */ |
Referenced by qt_set_parameters().
#define DEF_QT_POS_RECAL_DELAY 3u |
#define DEF_QT_RECAL_THRESHOLD RECAL_50 /* recal threshold = 50% of detect */ |
#define NUM_X_LINES 5 |
Define the Number X lines to be used.
Possible values: 4 and 8 Depending on the library used.Please refer to the QTouch library user guide.pdf and library selection guide.xls more information on selecting the number of channels.
#define NUM_X_PORTS 2 |
Specify the number of ports on which X-lines that are distributed.
Note: Support is provided only for a maximum of 3 ports for X. ( Maximum possible value for NUM_X_PORTS is 3) Possible values: 1,2,3 Also, note that code memory increases with the number of ports used for X lines.
#define NUM_Y_LINES 4 |
Define the Number Y lines and port for YA, YB to be used.
Possible values: NUM_Y_LINES is 1, 2, 4 and 8 Depending on the library used. Please refer to the QTouch library user guide.pdf and library selection guide.xls for more information on selecting the number of channels, YA and YB ports.
#define PORT_NUM_1 1 |
#define PORT_NUM_2 2 |
#define PORT_SMP D |
Specify the port for SMP.
And Specify the pin for SMP on selected SMP port. Any GPIO pin not conflicting with the other touch pins used for the application
#define PORT_SMP D |
Specify the port for SMP.
And Specify the pin for SMP on selected SMP port. Any GPIO pin not conflicting with the other touch pins used for the application
#define PORT_X_1 D |
Specify Which ports have X lines on them.
These macros are used to conditionally compile in support for ports driving X lines.
#define PORT_X_2 B |
#define PORT_YA G |
#define PORT_YB F |
#define QT_DELAY_CYCLES 2 |
Example configuration based on option selected in project options.
For user configuration make changes to the custom user configuration section above. Info on the below configuration macros refer above notes. Delay cycles that determine the capacitance charge pulse width. Value of 0 will enable charge pulse width of 1 clock cycle, 1 will enable a width of 2 clock cycles and so on...
Possible values: 1,2,3,4,5,10,25
#define QT_DELAY_CYCLES 2 |
Example configuration based on option selected in project options.
For user configuration make changes to the custom user configuration section above. Info on the below configuration macros refer above notes. Delay cycles that determine the capacitance charge pulse width. Value of 0 will enable charge pulse width of 1 clock cycle, 1 will enable a width of 2 clock cycles and so on...
Possible values: 1,2,3,4,5,10,25
#define QT_MAX_NUM_ROTORS_SLIDERS 4 |
Referenced by Transmit_State().
#define QT_NUM_CHANNELS 32 |
Number of Channels(dependent on the library used and application requirement).
The least possible number more that the application needs. Please refer to the QTouch library user guide.pdf and library selection guide.xls more information on selecting the number of channels.
Possible values: 4, 8, 16, 32, 56, 64. in case of QMatrix.
Referenced by qt_avr477_filter_cb(), Set_QM_Burst_Lengths(), Transmit_Burst_Lengths(), Transmit_Ref(), Transmit_Sensor_Config(), Transmit_Sign_On(), Transmit_Signals(), and Transmit_State().
#define SHARED_YAYB 0 |
Specify if YA and YB share the same port.
Set the value of the below macro to '1' if the YA and YB pins are share in same port.
#define SMP_PIN 5 |
#define SMP_PIN 5 |
#define TICKS_PER_MS 15u /* (16MHz/1024)* (1/1000) */ |
Total ticks per msec.
TICKS_PER_MS = (CLK_FREQ/TIMER_PRESCALER)*(1/1000)
Referenced by init_timer_isr(), and Transmit_Global_Config().