Microchip® Advanced Software Framework

qdebug_transport.h File Reference
#include "touch_api.h"

Macros

#define INT(a, b)   ((a << 8) | b)
 
#define MESSAGE_START   0x1B
 
#define RX_BUFFER_SIZE   (QT_NUM_CHANNELS*4)+10
 
#define STATE_DATA   3
 
#define STATE_IDLE   0
 
#define STATE_LENGTH1   1
 
#define STATE_LENGTH2   2
 
#define TX_BUFFER_SIZE   (QT_NUM_CHANNELS*4)+10
 

Functions

uint8_t GetChar (void)
 Get one byte from the Receive BufferRX_index is post incremented. More...
 
void Init_Buffers (void)
 Initialize the send and receive buffers. More...
 
void PutChar (uint8_t data)
 Puts one byte in the Transmit BufferTX_index is post incremented. More...
 
void PutInt (uint16_t data)
 Puts two bytes in the Transmit BufferBig Endian. More...
 
uint8_t RxHandler (uint8_t c)
 Handles the incomming bytes from the interface selected in QDebugSettings.h and puts the bytes in the RX_BufferUsed by SPI and TWI receive handlers. More...
 
void Send_Message (void)
 Send the content of the TX_Buffer to the USB Bridge using the interface selected in QDebugSettings.hCalled from the transmit functions in QDebug.c. More...
 
void Set_datamode (unsigned char mode)
 

Variables

unsigned int gMsTimeout
 
uint8_t RX_Buffer [RX_BUFFER_SIZE]
 
uint16_t RX_index
 
uint8_t SequenceH
 
uint8_t SequenceL
 
uint8_t TX_Buffer [TX_BUFFER_SIZE]
 
uint16_t TX_index
 

#define INT (   a,
 
)    ((a << 8) | b)
#define MESSAGE_START   0x1B

Referenced by Init_Buffers(), and RxHandler().

#define RX_BUFFER_SIZE   (QT_NUM_CHANNELS*4)+10
#define STATE_DATA   3

Referenced by RxHandler().

#define STATE_IDLE   0

Referenced by RxHandler().

#define STATE_LENGTH1   1

Referenced by RxHandler().

#define STATE_LENGTH2   2

Referenced by RxHandler().

#define TX_BUFFER_SIZE   (QT_NUM_CHANNELS*4)+10

void Init_Buffers ( void  )

Initialize the send and receive buffers.

Called from QDebug_Init

References MESSAGE_START, and TX_Buffer.

Referenced by QDebug_Init().

void Set_datamode ( unsigned char  mode)

unsigned int gMsTimeout
uint8_t RX_Buffer[RX_BUFFER_SIZE]
uint16_t RX_index
uint8_t SequenceH

Referenced by QDebug_SendData().

uint8_t SequenceL
uint8_t TX_Buffer[TX_BUFFER_SIZE]

Referenced by Init_Buffers().

uint16_t TX_index