This file contains the QTouch Libary configuration options for AVR 8-bit QMatrix method Capacitive Touch acquisition.
#include "touch_config.h"
Macros | |
#define | CLAMP_TO_DISCHARGE_TIME (DWELL_TIME_CYCLES -1) |
#define | DELAY_DWELL_TIME (DWELL_TIME_CYCLES -1) |
Set actual delay time in capacitive charge loop based on dwell time. More... | |
#define | DELAY_PRECHARGE_TIME (DWELL_TIME_CYCLES -1) |
#define | DELAY_X_DISCHARGE 0 |
#define | DWELL_TIME_CYCLES 2 |
Setting dwell time in cycles, and an empirical discharge delay to give c.50% duty cycle x pulses for the longer pulses. More... | |
#define | SMP_BIT SMP_PIN |
Warning: Please donot edit below this line. More... | |
#define CLAMP_TO_DISCHARGE_TIME (DWELL_TIME_CYCLES -1) |
#define DELAY_DWELL_TIME (DWELL_TIME_CYCLES -1) |
Set actual delay time in capacitive charge loop based on dwell time.
The -1 is because the following instruction in the charge transfer routine takes one cycle.
#define DELAY_PRECHARGE_TIME (DWELL_TIME_CYCLES -1) |
#define DELAY_X_DISCHARGE 0 |
#define DWELL_TIME_CYCLES 2 |
Setting dwell time in cycles, and an empirical discharge delay to give c.50% duty cycle x pulses for the longer pulses.
For the shorter ones, the spread spectrum calculations mean that we can't get the pulse low time down short enough for 50%.
#define SMP_BIT SMP_PIN |
Warning: Please donot edit below this line.
In case of Xmega devices, the mask is used instead of the pin number.