Microchip® Advanced Software Framework

avr32/applications/uc3-l0_xplained-demo/touch_config_at32uc3l.h File Reference

Touch library configuration.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

Macros

#define AT_SP_SELECTED   (SP15)
 Autonomous QTouch Clock dependency note: The Example application uses a PBA clock of 48MHz. More...
 
#define SET_PIN(x)   (1u << (x))
 Helper macro to include a selected pin. More...
 
Acquisition method manifest constants.

The following constants can be used to select the desired Touch acquisition methods to be used with the UC3L QTouch Library.

Choose QMatrix, Autonomous QTouch, QTouch Group A and QTouch Group B methods by setting the corresponding macro to 1. It is possible for the QTouch Library to support one or more acquisition methods at the same time. For example, in order to use QMatrix and Autonomous QTouch acquisition methods at the same time, both DEF_TOUCH_QMATRIX and DEF_TOUCH_AUTONOMOUS_QTOUCH macros must be set to 1.

#define DEF_TOUCH_QMATRIX   (1)
 When 1, QMatrix method acquisition is used. More...
 
#define DEF_TOUCH_AUTONOMOUS_QTOUCH   (1)
 When 1, Autonomous QTouch method acquisition is used. More...
 
#define DEF_TOUCH_QTOUCH_GRP_A   (0)
 When 1, QTouch Group A method acquisition is used. More...
 
#define DEF_TOUCH_QTOUCH_GRP_B   (0)
 When 1, QTouch Group B method acquisition is used. More...
 
#define DEF_TOUCH_QDEBUG_ENABLE_QM   (1)
 When 1, QMatrix debug data via QDebug is enabled When 0, QMatrix debug data via QDebug is disabled. More...
 
#define DEF_TOUCH_QDEBUG_ENABLE_AT   (0)
 When 1, Autonomous QTouch debug data via QDebug is enabled When 0, Autonomous QTouch debug data via QDebug is disabled. More...
 
#define DEF_TOUCH_QDEBUG_ENABLE_QTA   (0)
 When 1, QTouch Group A debug data via QDebug is enabled When 0, QTouch Group A debug data via QDebug is disabled. More...
 
#define DEF_TOUCH_QDEBUG_ENABLE_QTB   (0)
 When 1, QTouch Group B debug data via QDebug is enabled When 0, QTouch Group B debug data via QDebug is disabled. More...
 
#define DEF_TOUCH_QDEBUG_ENABLE
 When 1, QDebug debug data communication to QTouch Studio is enabled. More...
 
QMatrix Sensor Configuration options.

QMatrix Clock dependency note.

The Example application uses a PBA clock of 48MHz. When the UC3L PBA Clock is changed to a different frequency, the following parameters must be changed accordingly to ensure proper QMatrix operation.

  1. QM_GCLK_CAT_DIV.
  2. QM_CAT_CLK_DIV.
  3. TOUCH_SPREAD_SPECTRUM_MAX_DEV when Spread spectrum is enabled.

QMatrix resource requirement note. Caution:

  1. The QMatrix method acquisition using the CAT module uses the Analog comparators, controlled by the ACIFB. When QMatrix method acquisition is enabled, the Analog comparators should not be used by the user application at any given time.
  2. The QMatrix method acquisition using the CAT module requires two Peripheral DMA channels that must be provided by the application.
#define QM_NUM_X_LINES   (4u)
 QMatrix number of X Lines. More...
 
#define QM_NUM_Y_LINES   (1u)
 QMatrix number of Y Lines. More...
 
#define QM_NUM_SENSORS   (1u)
 QMatrix number of Sensors. More...
 
#define QM_NUM_ROTORS_SLIDERS   (4u)
 QMatrix number of Rotors and Sliders. More...
 
QMatrix Pin Configuration Options.
#define QM_X_PINS_SELECTED
 QMatrix X Pins selected. More...
 
#define QM_Y_PAIRS_SELECTED   SET_PIN(Y3_YK3)
 QMatrix Y-Yk Sense pairs selected. More...
 
#define QM_SMP_DIS_PIN_OPTION   (USE_NO_PIN)
 QMatrix SMP or DIS pin option. More...
 
#define QM_VDIV_PIN_OPTION   (USE_NO_PIN)
 QMatrix VDIV Pin option. More...
 
QMatrix Clock and Register Configuration Options.
#define QM_GCLK_CAT_DIV   (32u)
 QMatrix Generic clock (GCLK_CAT) divider for CAT. More...
 
#define QM_CAT_CLK_DIV   (5u)
 QMatrix CAT burst timing clock. More...
 
#define QM_CHLEN   (3u)
 QMatrix Charge Length. More...
 
#define QM_SELEN   (3u)
 QMatrix Settle Length. More...
 
#define QM_CXDILEN   (3u)
 QMatrix Cx Capacitor Discharge Length. More...
 
#define QM_DILEN   (255u)
 QMatrix Discharge Length. More...
 
#define QM_DISHIFT   (0u)
 QMatrix Discharge Shift. More...
 
#define QM_MAX_ACQ_COUNT   (6000u)
 QMatrix Maximum Count. More...
 
#define QM_CONSEN   (5u)
 QMatrix Consensus Filter Length. More...
 
#define QM_INTREFSEL   (1u)
 QMatrix Internal Reference Select. More...
 
#define QM_INTVREFSEL   (1u)
 QMatrix Internal Voltage Reference select. More...
 
#define QM_ENABLE_SPREAD_SPECTRUM   (1u)
 QMatrix Spread Spectrum Sensor Drive for QMatrix. More...
 
#define QM_ENABLE_EXTERNAL_SYNC   (0u)
 QMatrix External synchronization to reduce 50 or 60 Hz mains interference. More...
 
#define QM_SYNC_TIM   (0u)
 QMatrix Sync Time Interval. More...
 
QMatrix DMA Channel Options.
#define QM_DMA_CHANNEL_0   (0u)
 QMatrix DMA Channel 0. More...
 
#define QM_DMA_CHANNEL_1   (1u)
 QMatrix DMA Channel 1. More...
 
QMatrix Global acquisition parameters.

Refer the Touch Library User guide for more information on these parameters.

#define QM_DI   (4u)
 QMatrix Sensor detect integration (DI) limit. More...
 
#define QM_NEG_DRIFT_RATE   (20u)
 QMatrix Sensor negative drift rate. More...
 
#define QM_POS_DRIFT_RATE   (5u)
 QMatrix Sensor positive drift rate. More...
 
#define QM_MAX_ON_DURATION   (0u)
 QMatrix Sensor maximum on duration. More...
 
#define QM_DRIFT_HOLD_TIME   (20u)
 QMatrix Sensor drift hold time. More...
 
#define QM_POS_RECAL_DELAY   (10u)
 QMatrix Positive Recalibration delay. More...
 
#define QM_RECAL_THRESHOLD   (RECAL_50)
 QMatrix Sensor recalibration threshold. More...
 
QMatrix Callback functions.
#define QM_FILTER_CALLBACK   (NULL)
 QMatrix Filter callback function. More...
 
Autonomous QTouch Clock and Register Configuration Options.
#define AT_CAT_CLK_DIV   (23u)
 Autonomous QTouch burst timing clock Divider. More...
 
#define AT_CHLEN   (2u)
 Autonomous QTouch Charge Length For Autonomous QTouch sensor, specifies how many burst prescaler clock cycles should be used for transferring charge to the sense capacitor. More...
 
#define AT_SELEN   (1u)
 Autonomous QTouch Settle Length. More...
 
#define AT_DILEN   (255u)
 Autonomous QTouch Discharge Length. More...
 
#define AT_DISHIFT   (0u)
 Autonomous QTouch Discharge Shift. More...
 
#define AT_MAX_ACQ_COUNT   (3000u)
 Autonomous QTouch Maximum Count. More...
 
#define AT_ENABLE_SPREAD_SPECTRUM   (1u)
 Autonomous QTouch Spread Spectrum Sensor Drive. More...
 
#define AT_ENABLE_EXTERNAL_SYNC   (0u)
 Autonomous QTouch External synchronization to reduce 50 or 60 Hz mains interference. More...
 
#define AT_FILTER   (2u)
 Autonomous Touch Filter Setting. More...
 
#define AT_OUTSENS   (8u)
 Autonomous Touch Out-of-Touch Sensitivity. More...
 
#define AT_SENSE   (15u)
 Autonomous Touch Sensitivity. More...
 
#define AT_PTHR   (5u)
 Autonomous Touch Positive Recalibration Threshold. More...
 
#define AT_PDRIFT   (60u)
 Autonomous Touch Positive Drift Compensation. More...
 
#define AT_NDRIFT   (60u)
 Autonomous Touch Negative Drift Compensation. More...
 
Touch common configuration options.
#define TOUCH_SYNC_PIN_OPTION   (USE_NO_PIN)
 Touch Sync Pin option. More...
 
#define TOUCH_SPREAD_SPECTRUM_MAX_DEV   (4u)
 Touch Maximum Deviation. More...
 
#define TOUCH_CSARES   (0x00000400u)
 Touch Resistive Drive Enable for CSA lines. More...
 
#define TOUCH_CSBRES   (0x000094C0u)
 Touch Resistive Drive Enable for CSB lines. More...
 

#define AT_CAT_CLK_DIV   (23u)

Autonomous QTouch burst timing clock Divider.

The prescaler value is used to ensure that the CAT module clock (CLK_CAT) is divided to around 1 MHz to produce the burst timing clock. The prescaler uses the following formula to generate the burst timing clock: Burst timing clock = CLK_CAT / (2(DIV+1)). Range: 0u to 65535u.

#define AT_CHLEN   (2u)

Autonomous QTouch Charge Length For Autonomous QTouch sensor, specifies how many burst prescaler clock cycles should be used for transferring charge to the sense capacitor.

Units: Burst timing clock Range: 0u to 255u.

#define AT_DILEN   (255u)

Autonomous QTouch Discharge Length.

For Autonomous QTouch sensor, specifies how many burst prescaler clock cycles the CAT should use to discharge the capacitors before charging them. Units: Burst timing clock Range: 0u to 255u.

#define AT_DISHIFT   (0u)

Autonomous QTouch Discharge Shift.

For Autonomous QTouch sensor, specifies how many bits the DILEN field should be shifted before using it to determine the discharge time. Range: 0u to 3u.

#define AT_ENABLE_EXTERNAL_SYNC   (0u)

Autonomous QTouch External synchronization to reduce 50 or 60 Hz mains interference.

0u: For Autonomous QTouch sensor, specifies that external synchronization is disabled. 1u: For Autonomous QTouch sensor, specifies that external synchronization mode is enabled using the TOUCH_SYNC_PIN_OPTION pin option provided. Refer TOUCH_SYNC_PIN_OPTION option.

#define AT_ENABLE_SPREAD_SPECTRUM   (1u)

Autonomous QTouch Spread Spectrum Sensor Drive.

0u: For Autonomous QTouch sensor, specifies that spread spectrum sensor drive shall not be used. 1u: For Autonomous QTouch sensor, specifies that spread spectrum sensor drive shall be used.

#define AT_FILTER   (2u)

Autonomous Touch Filter Setting.

For the autonomous QTouch sensor, specifies how many positive detects in a row the CAT needs to have on the autonomous QTouch sensor before reporting it as a touch. Note: A FILTER value of 0 is not allowed and will result in undefined behavior. Range: 1u to 15u.

#define AT_MAX_ACQ_COUNT   (3000u)

Autonomous QTouch Maximum Count.

For Autonomous QTouch sensor, specifies how many counts (signal value) the maximum acquisition should be. Range: 0u to 65535u.

#define AT_NDRIFT   (60u)

Autonomous Touch Negative Drift Compensation.

For the autonomous QTouch sensor, specifies how often a negative drift compensation should be performed. When this field is zero, negative drift compensation will never be performed. When this field is non-zero, the negative drift compensation time interval is given by the following formula: Tndrift = NDRIFT * 65536 * (sample clock period) Range: 0u to 255u.

#define AT_OUTSENS   (8u)

Autonomous Touch Out-of-Touch Sensitivity.

For the autonomous QTouch sensor, specifies how sensitive the out-of-touch detector should be. When the sensor is not touched, the Autonomous Touch Current count register is same as the Autonomous Touch Base count register. When the sensor is touched the Autonomous Touch Current count register decreases. When using the Autonomous QTouch in proximity mode, the Autonomous Touch Base count register decreases as we move towards proximity of the sensor. The OUTSENS value can be arrived at by watching the CAT Autonomous Touch Base Count Register(at memory location 0xFFFF686Cu) and Autonomous Touch Current Count Register(at memory location 0xFFFF6870u) during a sensor touch/proximity and not in touch/proximity. A smaller difference between the Autonomous Touch Base count and Autonomous Touch Current count register can be chosen as the OUTSENS value. Range: 0u to 255u.

#define AT_PDRIFT   (60u)

Autonomous Touch Positive Drift Compensation.

For the autonomous QTouch sensor, specifies how often a positive drift compensation should be performed. When this field is zero, positive drift compensation will never be performed. When this field is non-zero, the positive drift compensation time interval is given by the following formula: Tpdrift = PDRIFT * 65536 * (sample clock period). Range: 0u to 255u.

#define AT_PTHR   (5u)

Autonomous Touch Positive Recalibration Threshold.

For the autonomous QTouch sensor, specifies how far a sensor's signal must move in a positive direction from the reference in order to cause a recalibration. Range: 0u to 255u.

#define AT_SELEN   (1u)

Autonomous QTouch Settle Length.

For Autonomous QTouch sensor, specifies how many burst prescaler clock cycles should be used for settling after charge transfer. Units: Burst timing clock Range: 0u to 255u.

#define AT_SENSE   (15u)

Autonomous Touch Sensitivity.

For the autonomous QTouch sensor, specifies how sensitive the touch detector should be. When the sensor is not touched, the Autonomous Touch Current count register is same as the Autonomous Touch Base count register. When the sensor is touched the Autonomous Touch Current count register decreases. When using the Autonomous QTouch in proximity mode, the Autonomous Touch Base count register decreases as we move towards proximity of the sensor. The SENSE value can be arrived at by watching the CAT Autonomous Touch Base Count Register(at memory location 0xFFFF686Cu) and Autonomous Touch Current Count Register(at memory location 0xFFFF6870u) during a sensor touch/proximity and not in touch/proximity. A larger difference between the Autonomous Touch Base count and Autonomous Touch Current count register can be chosen as the SENSE value. Range: 1u to 255u.

#define AT_SP_SELECTED   (SP15)

Autonomous QTouch Clock dependency note: The Example application uses a PBA clock of 48MHz.

When the UC3L PBA Clock is changed to a different frequency, the following parameters must be changed accordingly to ensure proper QMatrix operation.

  1. AT_CAT_CLK_DIV.
  2. TOUCH_SPREAD_SPECTRUM_MAX_DEV when Spread spectrum is enabled.

Autonomous QTouch Sensor Tuning Guide: When we start to tune the Proximity sensor, the values of AT_OUTSENS and AT_SENSE must be kept large. For example, AT_OUTSENS = 40u, AT_SENSE=80u. This will ensure that we do NOT hit the touch_at_status_change_interrupt_callback(), while we tune. With this setting, the Autonomous Touch Base Count Register (at memory location 0xFFFF686Cu) and Autonomous Touch Current Count Register (at memory location 0xFFFF6870u) should be watched using the IDE Memory window. In a "no Touch" situation, the two memory addresses should read similar values. Expect these values to be at least few tens. When the sensor is touched, the Current count register should decrease with respect to the base count register. In order to increase the count, one could try increasing the AT_CHLEN and AT_SELEN. Once we see this behavior, we can then tune the AT_OUTSENS and AT_SENSE as desired, and this should result in proper interrupts. Also, please ensure that you are using Rev D UC3L chip and not Rev B. With the RevB has few know issue on the Autonomous Touch. A smaller difference between the Autonomous Touch Base count and Autonomous Touch Current count register can be chosen as the OUTSENS value. A larger difference between the Autonomous Touch Base count and Autonomous Touch Current count register can be chosen as the SENSE value. Autonomous QTouch Sense pair selected. Specify the Sense pair to be used for Autonomous QTouch. Choose any ONE Sense Pair from SP0 to SP16. Specify the Sense pair SPn directly. Do NOT use the SET_PIN() macro when specifying the Sense pair. Refer qt_pin_options_t enum in touch_api_at32uc3l.h file.

#define DEF_TOUCH_AUTONOMOUS_QTOUCH   (1)

When 1, Autonomous QTouch method acquisition is used.

When 0, Autonomous QTouch method acquisition is not used.

#define DEF_TOUCH_QDEBUG_ENABLE
Value:
#define DEF_TOUCH_QDEBUG_ENABLE_AT
When 1, Autonomous QTouch debug data via QDebug is enabled When 0, Autonomous QTouch debug data via Q...
Definition: avr32/applications/uc3-l0_xplained-demo/touch_config_at32uc3l.h:79
#define DEF_TOUCH_QDEBUG_ENABLE_QM
When 1, QMatrix debug data via QDebug is enabled When 0, QMatrix debug data via QDebug is disabled...
Definition: avr32/applications/uc3-l0_xplained-demo/touch_config_at32uc3l.h:75
#define DEF_TOUCH_QDEBUG_ENABLE_QTA
When 1, QTouch Group A debug data via QDebug is enabled When 0, QTouch Group A debug data via QDebug ...
Definition: avr32/applications/uc3-l0_xplained-demo/touch_config_at32uc3l.h:83
#define DEF_TOUCH_QDEBUG_ENABLE_QTB
When 1, QTouch Group B debug data via QDebug is enabled When 0, QTouch Group B debug data via QDebug ...
Definition: avr32/applications/uc3-l0_xplained-demo/touch_config_at32uc3l.h:87

When 1, QDebug debug data communication to QTouch Studio is enabled.

When 0, QDebug debug data communication to QTouch Studio is disabled.

#define DEF_TOUCH_QDEBUG_ENABLE_AT   (0)

When 1, Autonomous QTouch debug data via QDebug is enabled When 0, Autonomous QTouch debug data via QDebug is disabled.

#define DEF_TOUCH_QDEBUG_ENABLE_QM   (1)

When 1, QMatrix debug data via QDebug is enabled When 0, QMatrix debug data via QDebug is disabled.

#define DEF_TOUCH_QDEBUG_ENABLE_QTA   (0)

When 1, QTouch Group A debug data via QDebug is enabled When 0, QTouch Group A debug data via QDebug is disabled.

#define DEF_TOUCH_QDEBUG_ENABLE_QTB   (0)

When 1, QTouch Group B debug data via QDebug is enabled When 0, QTouch Group B debug data via QDebug is disabled.

#define DEF_TOUCH_QMATRIX   (1)

When 1, QMatrix method acquisition is used.

When 0, QMatrix method acquisition is not used.

#define DEF_TOUCH_QTOUCH_GRP_A   (0)

When 1, QTouch Group A method acquisition is used.

When 0, QTouch Group A method acquisition is not used.

#define DEF_TOUCH_QTOUCH_GRP_B   (0)

When 1, QTouch Group B method acquisition is used.

When 0, QTouch Group B method acquisition is not used.

#define QM_CAT_CLK_DIV   (5u)

QMatrix CAT burst timing clock.

The prescaler value is used to ensure that the CAT module clock (CLK_CAT) is divided to around 4 MHz to produce the burst timing clock. The prescaler uses the following formula to generate the burst timing clock: Burst timing clock = CLK_CAT / (2(DIV+1)) Range: 0u to 255u.

#define QM_CHLEN   (3u)

QMatrix Charge Length.

For QMatrix sensors, specifies how many burst prescaler clock cycles should be used for transferring charge to the sense capacitor. Units: Burst timing clock Range: 0u to 255u.

#define QM_CONSEN   (5u)

QMatrix Consensus Filter Length.

For QMatrix sensors, specifies that discharge will be terminated when CONSEN out of the most recent 5 comparator samples are positive. For example, a value of 3 in the CONSEN field will terminate discharge when 3 out of the most recent 5 comparator samples are positive. When CONSEN has the default value of 0, discharge will be terminated immediately when the comparator output goes positive. Range: 0u to 5u.

#define QM_CXDILEN   (3u)

QMatrix Cx Capacitor Discharge Length.

For QMatrix sensors, specifies how many burst prescaler clock cycles the CAT should use to discharge the Cx capacitor at the end of each burst cycle. Units: Burst timing clock Range: 0u to 255u.

#define QM_DI   (4u)

QMatrix Sensor detect integration (DI) limit.

Range: 0u to 255u.

#define QM_DILEN   (255u)

QMatrix Discharge Length.

For QMatrix sensors, specifies how many burst prescaler clock cycles the CAT should use to discharge the capacitors at the beginning of a burst sequence. Units: Burst timing clock Range: 0u to 255u.

#define QM_DISHIFT   (0u)

QMatrix Discharge Shift.

For QMatrix sensors, specifies how many bits the DILEN field should be shifted before using it to determine the discharge time. Range: 0u to 3u.

#define QM_DMA_CHANNEL_0   (0u)

QMatrix DMA Channel 0.

Specify the DMA Channel option 0 to be used by the CAT module for transfer of Acquisition count from CAT register to memory. A different combination of DMA Channel option 0 and DMA Channel option 1 can be provided for each touch_qm_sensors_start_acquisition API call. Range: 0u to 11u. Note: DMA Channel option 0 and DMA Channel option 1 cannot be the same.

#define QM_DMA_CHANNEL_1   (1u)

QMatrix DMA Channel 1.

Specify the DMA Channel option 1 to be used by the CAT module for transfer of burst length values from memory to CAT register. A different combination of DMA Channel option 0 and DMA Channel option 1 can be provided for each touch_qm_sensors_start_acquisition API call. Range: 0u to 11u. Note: DMA Channel option 0 and DMA Channel option 1 cannot be the same.

#define QM_DRIFT_HOLD_TIME   (20u)

QMatrix Sensor drift hold time.

Units: 200ms Default value: 20 (hold off drifting for 4 seconds after leaving detect). Range: 1u to 255u.

#define QM_ENABLE_EXTERNAL_SYNC   (0u)

QMatrix External synchronization to reduce 50 or 60 Hz mains interference.

0u: For QMatrix sensors, specifies that external synchronization is disabled. 1u: For QMatrix sensors, specifies that external synchronization mode is enabled using the TOUCH_SYNC_PIN_OPTION pin option provided. Refer TOUCH_SYNC_PIN_OPTION option.

#define QM_ENABLE_SPREAD_SPECTRUM   (1u)

QMatrix Spread Spectrum Sensor Drive for QMatrix.

0u: For QMatrix sensors, specifies that spread spectrum sensor drive shall not be used. 1u: For QMatrix sensors, specifies that spread spectrum sensor drive shall be used.

#define QM_FILTER_CALLBACK   (NULL)

QMatrix Filter callback function.

A filter callback (when not NULL) is called by the Touch Library each time a new set of Signal values are available. An Example filter callback function prototype. void qm_filter_callback( touch_filter_data_t *p_filter_data );

#define QM_GCLK_CAT_DIV   (32u)

QMatrix Generic clock (GCLK_CAT) divider for CAT.

For proper QMatrix operation, the frequency of GCLK_CAT <= (PBA Clock/4). Range: 0u to 65535u. Note: The range specified is valid when this macro is used in conjunction with scif_gc_setup() API. Refer clock.c file. Note: This option is common for QMatrix, QTouch and Autonomous Touch methods of acquisition.

#define QM_INTREFSEL   (1u)

QMatrix Internal Reference Select.

This option is valid only when using the internal current sources mode of discharging the capacitors. 0u: The reference current flows through an external resistor on the DIS pin. 1u: The reference current flows through the internal reference resistor.

#define QM_INTVREFSEL   (1u)

QMatrix Internal Voltage Reference select.

This option is valid only when using the internal current sources mode of discharging the capacitors. 0u: The voltage for the reference resistor is generated from the internal band gap circuit. 1u: The voltage for the reference resistor is VDDIO/2.

#define QM_MAX_ACQ_COUNT   (6000u)

QMatrix Maximum Count.

For QMatrix sensors, specifies how many counts (signal value) the maximum acquisition should be. Range: 0u to 65535u.

#define QM_MAX_ON_DURATION   (0u)

QMatrix Sensor maximum on duration.

Units: 200ms (Example: a value 5u indicated Max ON duration of 1 second.) Default value: 0 (No maximum ON time limit). Range: 0u to 255u.

#define QM_NEG_DRIFT_RATE   (20u)

QMatrix Sensor negative drift rate.

Units: 200ms Default value: 20u = 4 seconds. Range: 1u to 127u.

#define QM_NUM_ROTORS_SLIDERS   (4u)

QMatrix number of Rotors and Sliders.

Specify the total number of QMatrix Rotors and Sliders to be used by the Touch Library. The number of Rotors and Sliders mentioned here is part of the Total number of sensors specified in the QM_NUM_SENSORS macro. Note: When no rotors or slider are required, specify a value of 0u.

#define QM_NUM_SENSORS   (1u)

QMatrix number of Sensors.

Specify the number of QMatrix touch sensors to be used by the Touch Library. A sensor can be a key, rotor or slider. Example configuration: If the configuration has 6 keys (a key is formed using one channel), one rotor (a QMatrix rotor is formed using 3 to 8 channels) and one slider (a QMatrix slider is formed using 3 to 8 channels), then the number of sensors is 6 key + 1 rotor + 1 slider = 8 sensors. Range: 1u to (number of X Lines * number of Y_Yk pairs).

#define QM_NUM_X_LINES   (4u)

QMatrix number of X Lines.

Specify the number of QMatrix X Lines to be used by the Touch Library. Refer CAT Matrix Connections Figure 28-2 in the datasheet. Range: 1u to 17u.

#define QM_NUM_Y_LINES   (1u)

QMatrix number of Y Lines.

Specify the number of QMatrix Y-Yk pair to be used by the Touch Library. Refer CAT Matrix Connections Figure 28-2 in the datasheet. Range: 1u to 8u.

#define QM_POS_DRIFT_RATE   (5u)

QMatrix Sensor positive drift rate.

Units: 200ms Default value: 5u = 1 second. Range: 1u to 127u.

#define QM_POS_RECAL_DELAY   (10u)

QMatrix Positive Recalibration delay.

Default value: 10. Range: 1u to 255u.

#define QM_RECAL_THRESHOLD   (RECAL_50)

QMatrix Sensor recalibration threshold.

Default: RECAL_50 (recalibration threshold = 50% of detection threshold). Range: refer recal_threshold_t enum in touch_api_at32uc3l.h.

#define QM_SELEN   (3u)

QMatrix Settle Length.

For QMatrix sensors, specifies how many burst prescaler clock cycles should be used for settling after charge transfer. Units: Burst timing clock Range: 0u to 255u.

#define QM_SMP_DIS_PIN_OPTION   (USE_NO_PIN)

QMatrix SMP or DIS pin option.

Specify the smp or dis pin option, if included in the hardware design. The QMatrix hardware can use a SMP pin for the discharge of the capacitors. In this arrangement, a logic-level (SMP) pin is connected to the capacitors through external high value resistors (typically between 100 kohm and 1 Megohm). When this arrangement is used, one of the SMP pin option must be chosen from the list available in the general_pin_options_t enum.

Alternatively, the UC3L CAT module provides an option of using the internal current sources for the discharge of capacitors. By choosing this hardware arrangement, the external resistors to be used with the SMP method can be avoided. The discharge of capacitors in this method can be done in two ways. If the INTREFSEL macro is set to 1, then a internal resistor shall be used to discharge the current. If the INTREFSEL macro is set to 0, then a external resistor shall be used to discharge the current. When the INTREFSEL=0 external discharge mode arrangement is used, one of the DIS pin option must be chosen from the list available in the general_pin_options_t enum. When the INTREFSEL=1 internal discharge mode arrangement is used, the USE_NO_PIN option must be specified for the QM_SMP_DIS_PIN_OPTION.

Refer general_pin_options_t enum in touch_api_at32uc3l.h file. Also, refer macros QM_INTREFSEL and QM_INTVREFSEL. Also, refer CAT Matrix Connections Figure 28-2 in the datasheet.

#define QM_SYNC_TIM   (0u)

QMatrix Sync Time Interval.

When non-zero, determines the number of prescaled clock cycles between the start of the acquisition on each X line for QMatrix acquisition. This option is valid only in the case when QM_ENABLE_EXTERNAL_SYNC is enabled. Units: Burst timing clock Range: 0u to 4095u.

#define QM_VDIV_PIN_OPTION   (USE_NO_PIN)

QMatrix VDIV Pin option.

Specify the vdiv pin option, if included in the hardware design. The VDIV pin provides an option to make ACREFN a small positive voltage in the case of any analog comparator offset issues. The VDIV pin is driven when the analog comparators are in use, and this signal can be used along with a voltage divider arrangement to create a small positive offset on the ACREFN pin.

Refer general_pin_options_t enum in touch_api_at32uc3l.h file. Also, refer CAT Matrix Connections Figure 28-2 in the datasheet.

#define QM_X_PINS_SELECTED
Value:
#define SET_PIN(x)
Helper macro to include a selected pin.
Definition: avr32/applications/uc3-l0_xplained-demo/touch_config_at32uc3l.h:99
Definition: avr32/applications/uc3l-ek-touch-demo/touch_api_at32uc3l.h:472
Definition: avr32/applications/uc3l-ek-touch-demo/touch_api_at32uc3l.h:468
Definition: avr32/applications/uc3l-ek-touch-demo/touch_api_at32uc3l.h:474
Definition: avr32/applications/uc3l-ek-touch-demo/touch_api_at32uc3l.h:471

QMatrix X Pins selected.

Specify the X lines to be used. Choose from X0 to X17. Setting Bit'n' indicates that a pin Xn is selected. Use the SET_PIN() macro to select the required X pin. Refer x_pin_options_t enum in touch_api_at32uc3l.h file.

#define QM_Y_PAIRS_SELECTED   SET_PIN(Y3_YK3)

QMatrix Y-Yk Sense pairs selected.

Specify the Y pairs to be used. Choose from Y0_YK0 to Y7_YK7. Setting Bit'n' indicates that a pair Yn_YKn is selected. Use the SET_PIN() macro to select the required Yn_YKn pair. Refer y_pin_options_t enum in touch_api_at32uc3l.h file.

#define SET_PIN (   x)    (1u << (x))

Helper macro to include a selected pin.

#define TOUCH_CSARES   (0x00000400u)

Touch Resistive Drive Enable for CSA lines.

This option can be used to enable 1kOhm resistive drive capability, if available on a specific CSA pin. For the UC3L, the following CSA[n] pin have the resistive drive capability - CSARES: 0x0001AEEEu When bit n is 0, CSA[n] has the same drive properties as normal I/O pads. When bit n is 1, CSA[n] has a nominal output resistance of 1kOhm during the burst phase. Refer Table 28-2. Pin Selection Guide.

#define TOUCH_CSBRES   (0x000094C0u)

Touch Resistive Drive Enable for CSB lines.

This option can be used to enable 1kOhm resistive drive capability, if available on a specific CSA pin. For the UC3L, the following CSB[n] pin have the resistive drive capability - CSBRES: 0x0000BEECu When bit n is 0, CSB[n] has the same drive properties as normal I/O pads. When bit n is 1, CSB[n] has a nominal output resistance of 1kOhm during the burst phase. Refer Table 28-2. Pin Selection Guide.

#define TOUCH_SPREAD_SPECTRUM_MAX_DEV   (4u)

Touch Maximum Deviation.

When spread spectrum burst is enabled using the QM_ENABLE_SPREAD_SPECTRUM option, MAX_DEV indicates the maximum number of prescaled clock cycles the burst pulse will be extended or shortened. Range: When only QMatrix is used, 0u to ((2u * QM_CAT_CLK_DIV) + 1u). Range: When only Autonomous QTouch is used, 0u to ((2u * AT_CAT_CLK_DIV) + 1u). Range: When only QTouch Group A is used, 0u to ((2u * QTA_CAT_CLK_DIV) + 1u). Range: When only QTouch Group B is used, 0u to ((2u * QTB_CAT_CLK_DIV) + 1u). Range: When a combination of QMatrix, Autonomous QTouch, QTouch Group A or QTouch Group B is used, 0u to ((2u * least of(QM_CAT_CLK_DIV, AT_CAT_CLK_DIV, QTA_CAT_CLK_DIV, QTB_CAT_CLK_DIV )) + 1u)

#define TOUCH_SYNC_PIN_OPTION   (USE_NO_PIN)

Touch Sync Pin option.

Specify the sync pin option, if included in the hardware design. To prevent interference from the 50 or 60 Hz mains line the CAT can trigger acquisition on the SYNC signal. The SYNC signal should be derived from the mains line. The acquisition will trigger on a falling edge of this signal. Refer general_pin_options_t enum in touch_api_at32uc3l.h file.