Microchip® Advanced Software Framework

common/applications/sensors/inertial_wake/main.c File Reference

Common Sensor Service Inertial Sensor Wake Event Example.

Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.

#include <stdio.h>
#include <asf.h>
#include <led.h>

Macros

#define ACCEL_LED   LED1 /* LED to indicate accel interrupt */
 
#define ACCEL_MOT_THRESH   (250) /* Accel any-motion threshold (milli-g) */
 
#define ACCEL_WAKE   (true) /* If true, use accel any-motion to wake up */
 
#define ACTIVITY_LED   LED4 /* LED to show awake/operating */
 
#define GYRO_LED   LED3 /* LED to indicate gyro interrupt */
 
#define GYRO_RESTART_DELAY   (50) /* Gyro restart (after sleep) delay (msec) */
 
#define GYRO_SAMPLE_RATE   (100) /* Gyro sample rate (Hz) */
 
#define GYRO_SLEEP   (false) /* If true, put gyro in sleep mode */
 
#define GYRO_WAKE   (false) /* If true, use gyro new data to wake up */
 
#define SCALED_DATA   (true)
 
#define USE_ACCEL   (true) /* If true, init & read accel */
 
#define USE_GYRO   (false) /* If true, init & read gyro */
 
#define USE_PRINTF   (false)
 

Functions

static void acceleration_event (volatile sensor_event_data_t *event_data, volatile void *arg)
 
int main (void)
 Inertial sensor demo application entry. More...
 
static void rotation_event (volatile sensor_event_data_t *event_data, volatile void *arg)
 

Variables

volatile sensor_data_t acceleration = { .scaled = SCALED_DATA }
 
sensor_t accelerometer
 
sensor_t gyroscope
 
volatile sensor_data_t rotation = { .scaled = SCALED_DATA }
 

#define ACCEL_LED   LED1 /* LED to indicate accel interrupt */

Referenced by acceleration_event().

#define ACCEL_MOT_THRESH   (250) /* Accel any-motion threshold (milli-g) */

Referenced by main().

#define ACCEL_WAKE   (true) /* If true, use accel any-motion to wake up */
#define ACTIVITY_LED   LED4 /* LED to show awake/operating */

Referenced by main().

#define GYRO_LED   LED3 /* LED to indicate gyro interrupt */

Referenced by rotation_event().

#define GYRO_RESTART_DELAY   (50) /* Gyro restart (after sleep) delay (msec) */

Referenced by main().

#define GYRO_SAMPLE_RATE   (100) /* Gyro sample rate (Hz) */

Referenced by main().

#define GYRO_SLEEP   (false) /* If true, put gyro in sleep mode */
#define GYRO_WAKE   (false) /* If true, use gyro new data to wake up */
#define SCALED_DATA   (true)

Referenced by main().

#define USE_ACCEL   (true) /* If true, init & read accel */
#define USE_GYRO   (false) /* If true, init & read gyro */
#define USE_PRINTF   (false)

static void acceleration_event ( volatile sensor_event_data_t event_data,
volatile void *  arg 
)
static

Accelerometer Event Callback Routine

References ACCEL_LED, and sensor_event_data_t::data.

Referenced by main().

int main ( void  )

Inertial sensor demo application entry.

After initializing the Xplained platform and sensor boards, this application attaches descriptors to the accelerometer and gyroscope devices on an Xplained inertial sensor board. The sensor data, which is formatted and printed via printf() after being read, can be viewed with a serial terminal application on a machine attached to the USB interface on the Xplained board.

References ACCEL_MOT_THRESH, acceleration_event(), ACTIVITY_LED, sensor_data_t::axis, delay_ms, GYRO_RESTART_DELAY, GYRO_SAMPLE_RATE, rotation_event(), SCALED_DATA, sensor_add_event(), sensor_attach(), SENSOR_EVENT_MOTION, SENSOR_EVENT_NEW_DATA, sensor_get_rotation(), sensor_platform_init(), sensor_set_sample_rate(), sensor_set_state(), sensor_set_threshold(), SENSOR_STATE_LOW_POWER, SENSOR_STATE_NORMAL, SENSOR_STATE_SLEEP, SENSOR_THRESHOLD_MOTION, SENSOR_TYPE_ACCELEROMETER, SENSOR_TYPE_GYROSCOPE, sleepmgr_enter_sleep(), sleepmgr_init(), and sleepmgr_lock_mode().

static void rotation_event ( volatile sensor_event_data_t event_data,
volatile void *  arg 
)
static

Gyroscope Event Callback Routine

References sensor_event_data_t::data, and GYRO_LED.

Referenced by main().

volatile sensor_data_t acceleration = { .scaled = SCALED_DATA }
sensor_t accelerometer
sensor_t gyroscope
volatile sensor_data_t rotation = { .scaled = SCALED_DATA }