Microchip® Advanced Software Framework

common/applications/sensors/prox_gesture/main.c File Reference

Common Sensor Service Proximity Sensor Gesture Recognition Example.

Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.

#include <stdio.h>
#include <asf.h>
#include <led.h>

Macros

#define CHAN_1   0x01
 
#define CHAN_2   0x02
 
#define CHAN_3   0x04
 
#define CHAN_NONE   0x00
 
#define DOWN_LED   LED1
 
#define ERR_BLINK_COUNT   (2) /* Number of times to blink LEDs on error */
 
#define LEFT_LED   LED2
 
#define PROX_CURRENT_mA   (150) /* Current for proximity sensor LEDs (mA) */
 
#define PROX_SAMPLE_RATE   (100) /* Proximity sensor sample rate (Hz) */
 
#define PROX_THRESHOLD   (100) /* Manual prox sensor threshold for "near" */
 
#define RIGHT_LED   LED3
 
#define SET_PROX_CURRENT   (true) /* If true, manually set proximity current */
 
#define SET_PROX_THRESHOLD
 
#define UP_LED   LED0
 
#define USE_PRINTF
 

Enumerations

enum  direction_t {
  UNK = 0,
  UP = 1,
  DOWN = 2,
  LEFT = 3,
  RIGHT = 4
}
 Direction code values. More...
 

Functions

int main (void)
 Proximity Sensor gesture recognition demo application entry. More...
 
static void prox_event_handler (volatile sensor_event_data_t *event_data, volatile void *arg)
 Proximity event handler. More...
 
static int8_t test_channels (sensor_data_t *data)
 Proximity value test. More...
 

Variables

static const char *const channel_labels [8]
 Strings to indicate which channels detected proximity. More...
 
direction_t dir_tbl [8][8]
 Direction lookup table of start_channels (rows) x end_channels (columns) More...
 
static const char *const direction_labels [5]
 Strings to display based on gesture direction. More...
 
sensor_data_t prox_data = { .scaled = true }
 
sensor_t prox_dev
 
bool prox_event_occurred = false
 

#define CHAN_1   0x01

Referenced by test_channels().

#define CHAN_2   0x02

Referenced by test_channels().

#define CHAN_3   0x04

Referenced by test_channels().

#define CHAN_NONE   0x00

Referenced by main(), and test_channels().

#define DOWN_LED   LED1

Referenced by main().

#define ERR_BLINK_COUNT   (2) /* Number of times to blink LEDs on error */

Referenced by main().

#define LEFT_LED   LED2

Referenced by main().

#define PROX_CURRENT_mA   (150) /* Current for proximity sensor LEDs (mA) */

Referenced by main().

#define PROX_SAMPLE_RATE   (100) /* Proximity sensor sample rate (Hz) */

Referenced by main().

#define PROX_THRESHOLD   (100) /* Manual prox sensor threshold for "near" */

Referenced by main().

#define RIGHT_LED   LED3

Referenced by main().

#define SET_PROX_CURRENT   (true) /* If true, manually set proximity current */
#define SET_PROX_THRESHOLD
Value:
(true) /* If true, manually set proximity
* threshold */
#define UP_LED   LED0

Referenced by main().

#define USE_PRINTF
Value:
(true) /* If true, output results via serial
* terminal */

Direction code values.

Enumerator
UNK 
UP 
DOWN 
LEFT 
RIGHT 

int main ( void  )

Proximity Sensor gesture recognition demo application entry.

This application uses a 3-channel proximity sensor to recognize simple gestures. When a proximity event occurs, the routine will wake up from a low-power sleep mode and begin repeatedly sampling the proximity sensor, until the proximity of the object is no longer detected. Then the beginning and ending sensor readings are compared, and the overall direction of the object's movement is determined based on a lookup table.

Once the direction is determined, it is indicate by turning on one of the LEDs on the controller board and (optionally) by serial output to a terminal device. If the direction cannot be determined, all indicator LEDs will be blinked rapidly.

The application then resets by returning to a low-power sleep mode until the next proximity event is detected.

References CHAN_NONE, channel_labels, delay_ms, dir_tbl, direction_labels, DOWN, DOWN_LED, ERR_BLINK_COUNT, i, LEFT, LEFT_LED, PROX_CURRENT_mA, prox_event_handler(), prox_event_occurred, PROX_SAMPLE_RATE, PROX_THRESHOLD, RIGHT, RIGHT_LED, sensor_add_event(), sensor_attach(), SENSOR_CHANNEL_ALL, sensor_device_id(), sensor_disable_event(), sensor_enable_event(), SENSOR_EVENT_NEAR_PROXIMITY, sensor_get_proximity(), sensor_platform_init(), sensor_set_channel(), sensor_set_current(), sensor_set_sample_rate(), sensor_set_threshold(), SENSOR_THRESHOLD_NEAR_PROXIMITY, SENSOR_TYPE_PROXIMITY, sleepmgr_enter_sleep(), sleepmgr_init(), sleepmgr_lock_mode(), test_channels(), UP, UP_LED, and version.

static void prox_event_handler ( volatile sensor_event_data_t event_data,
volatile void *  arg 
)
static

Proximity event handler.

This routine will be called when a near-proximity event occurs. It simply copies the proximity data to the sensor_data_t structure specified during the sensor_add_event function call.

This routine executes as part of the interrupt service routine for the sensor interrupt.

References sensor_event_data_t::data, and prox_event_occurred.

Referenced by main().

static int8_t test_channels ( sensor_data_t data)
static

Proximity value test.

This routine examines the data fields in the sensor_data_t structure and returns a single value summarizing which channels have a reported proximity value (i.e. the value is not PROXIMITY_NONE).

Parameters
dataAddress of sensor_data_t struct containing prox data
Returns
int8_t Encoded with bits set per channel over threshold

References CHAN_1, CHAN_2, CHAN_3, CHAN_NONE, sensor_data_t::proximity, and PROXIMITY_NONE.

Referenced by main().

const char* const channel_labels[8]
static
Initial value:
= {
"none ",
"1 ",
"2 ",
"1+2 ",
"3 ",
"1+3 ",
"2+3 ",
"1+2+3"
}

Strings to indicate which channels detected proximity.

Referenced by main().

direction_t dir_tbl[8][8]
Initial value:
=
{{ UNK, UNK, UNK, UNK, UNK, UNK, UNK, UNK },
{ UNK, UNK, RIGHT, UNK, DOWN, UNK, DOWN, DOWN },
{ UNK, LEFT, UNK, UNK, LEFT, LEFT, UNK, LEFT },
{ UNK, UNK, UNK, UNK, DOWN, UNK, DOWN, UNK },
{ UNK, UP, RIGHT, UP, UNK, UNK, RIGHT, UP },
{ UNK, UP, RIGHT, RIGHT, DOWN, UNK, RIGHT, RIGHT },
{ UNK, UP, RIGHT, UP, LEFT, LEFT, UNK, UNK },
{ UNK, UP, RIGHT, UNK, DOWN, LEFT, UNK, UNK }}
Definition: common/applications/sensors/prox_gesture/main.c:126
Definition: common/applications/sensors/prox_gesture/main.c:127
Definition: common/applications/sensors/prox_gesture/main.c:125
Definition: common/applications/sensors/prox_gesture/main.c:128
Definition: common/applications/sensors/prox_gesture/main.c:124

Direction lookup table of start_channels (rows) x end_channels (columns)

Referenced by main().

const char* const direction_labels[5]
static
Initial value:
= {
"Unknown",
"Up ",
"Down ",
"Left ",
"Right "
}

Strings to display based on gesture direction.

Referenced by main().

sensor_data_t prox_data = { .scaled = true }

Referenced by main(), and sfh7770_calibrate().

sensor_t prox_dev

Referenced by main().

bool prox_event_occurred = false