Microchip® Advanced Software Framework

common/services/isp/flip/isp.h File Reference

In System Programming API.

Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.

#include "conf_isp.h"

Data Structures

struct  isp_mem_bootloader_t
 Memory bootloader structure. More...
 
struct  isp_mem_t
 Memory API definition. More...
 
union  isp_mems_t
 Memories list structure. More...
 

Macros

Memory units index values

Used to access at a memory through isp_memories list.

#define ISP_MEM_FLASH   0x00
 
#define ISP_MEM_EEPROM   0x01
 
#define ISP_MEM_SECURITY   0x02
 
#define ISP_MEM_CONFIGURATION   0x03
 
#define ISP_MEM_BOOTLOADER   0x04
 
#define ISP_MEM_SIGNATURE   0x05
 
#define ISP_MEM_USER   0x06
 
#define ISP_MEM_INT_RAM   0x07
 
#define ISP_MEM_EXT_MEM_CS0   0x08
 
#define ISP_MEM_EXT_MEM_CS1   0x09
 
#define ISP_MEM_EXT_MEM_CS2   0x0A
 
#define ISP_MEM_EXT_MEM_CS3   0x0B
 
#define ISP_MEM_EXT_MEM_CS4   0x0C
 
#define ISP_MEM_EXT_MEM_CS5   0x0D
 
#define ISP_MEM_EXT_MEM_CS6   0x0E
 
#define ISP_MEM_EXT_MEM_CS7   0x0F
 
#define ISP_MEM_EXT_MEM_DF   0x10
 
#define ISP_MEM_COUNT   0x11
 

Typedefs

typedef uint32_t isp_addr_t
 Data type for holding flash memory addresses. More...
 

Functions

 COMPILER_PACK_SET (1) typedef union
 Memory signature structure to store JTAG ID. More...
 
Main In System Programming functions
void isp_init (void)
 Initializes the ISP interface. More...
 
bool isp_is_security (void)
 Gives the security state of the chip. More...
 
void isp_force_boot_isp (bool force)
 Change the boot process configuration to enable/disable the ISP mode for the next startup. More...
 
bool isp_erase_chip (void)
 Erase the application flash area and eventually the eeprom. More...
 
bool isp_erase_chip_split (void)
 Erase a part of the application flash area This function must be called again as long as it returns 0. More...
 
void isp_start_appli (void)
 Resets the device to start the user application. More...
 

Variables

 isp_mem_signature_t
 
const isp_mems_t isp_memories
 Memories list declaration. More...