Sensor API device definitions.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include "sensor.h"
Macros | |
Sensor Device Bus Addresses | |
Each driver must have a bus address _bus_addr defined here, where is the same prefix used for the driver _init function. The bus address definitions are keyed off build constants and will vary by application. If the bus does not assign particular addresses, then define the address as (0). If, as is the case with TWI/I2C, the device responds to a specific address, then define the constant bus address value. The default values provided here may be modified or redefined by specific board and bus implementations. | |
#define | ak8975_bus_addr (0) |
#define | kxtf9_bus_addr (0) |
#define | hmc5883l_bus_addr (0) |
#define | bma020_bus_addr (0) |
#define | bma150_bus_addr (0) |
#define | bma180_bus_addr (0) |
#define | bma220_bus_addr (0) |
#define | bma222_bus_addr (0) |
#define | bma250_bus_addr (0) |
#define | bmp085_bus_addr (0) |
#define | bmp180_bus_addr (0) |
#define | imu3000_bus_addr (0) |
#define | itg3200_bus_addr (0) |
#define | sfh5712_bus_addr (0) |
#define | sfh7770_bus_addr (0) |
Functions | |
Sensor Driver Initialization Entry Points | |
bool | ak8975_init (sensor_t *, int) |
AKM AK8975 magnetometer driver initialization. More... | |
bool | bma020_init (sensor_t *, int) |
Bosch BMA020 accelerometer driver initialization. More... | |
bool | bma150_init (sensor_t *, int) |
Bosch BMA150 accelerometer driver initialization. More... | |
bool | bma180_init (sensor_t *, int) |
Bosch BMA180 accelerometer driver initialization. More... | |
bool | bma220_init (sensor_t *, int) |
Bosch BMA220 accelerometer driver initialization. More... | |
bool | bma222_init (sensor_t *, int) |
Bosch BMA222 accelerometer driver initialization. More... | |
bool | bma250_init (sensor_t *, int) |
Bosch BMA250 accelerometer driver initialization. More... | |
bool | bmp085_init (sensor_t *, int) |
Bosch BMP085 barometric sensor driver initialization. More... | |
bool | bmp180_init (sensor_t *, int) |
Bosch BMP180 barometric sensor driver initialization. More... | |
bool | hmc5883l_init (sensor_t *, int) |
Honeywell HMC5883L magnetometer driver initialization. More... | |
bool | imu3000_init (sensor_t *, int) |
InvenSense IMU-3000 motion processor driver initialization. More... | |
bool | itg3200_init (sensor_t *, int) |
InvenSense ITG-3200 gyroscope driver initialization. More... | |
bool | kxtf9_init (sensor_t *, int) |
Kionix KXTF9 accelerometer driver initialization. More... | |
bool | sfh5712_init (sensor_t *, int) |
Osram SFH5712 light sensor driver initialization. More... | |
bool | sfh7770_init (sensor_t *, int) |
Osram SFH7770 light & proximity sensor driver initialization. More... | |
#define ak8975_bus_addr (0) |
#define bma020_bus_addr (0) |
#define bma150_bus_addr (0) |
#define bma180_bus_addr (0) |
#define bma220_bus_addr (0) |
#define bma222_bus_addr (0) |
#define bma250_bus_addr (0) |
#define bmp085_bus_addr (0) |
#define bmp180_bus_addr (0) |
#define hmc5883l_bus_addr (0) |
#define imu3000_bus_addr (0) |
#define itg3200_bus_addr (0) |
#define kxtf9_bus_addr (0) |
#define sfh5712_bus_addr (0) |
#define sfh7770_bus_addr (0) |
AKM AK8975 magnetometer driver initialization.
This is the main initialization function for the AK8975 device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
References ak8975_calibrate(), AK8975_DATA_RESOLUTION, ak8975_ioctl(), ak8975_read(), AK8975_REG_WIA, ak8975_selftest(), AK8975_WIA_VALUE, sensor_device_t::func, nvram_read(), sensor_funcs_t::read, sensor_hal::resolution, sensor_bus_get, SENSOR_CAPS_3_AXIS, SENSOR_CAPS_SELFTEST, SENSOR_SCALE_micro, SENSOR_UNITS_tesla, SENSOR_VENDOR_AKM, vector3_t::x, vector3_t::y, and vector3_t::z.
Bosch BMA020 accelerometer driver initialization.
This is the main initialization function for the BMA020 device. The accelerometer range and bandwidth are set based on user-specified values from the system configuration.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
Bosch BMA150 accelerometer driver initialization.
This is the main initialization function for the BMA150 device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
Bosch BMA180 accelerometer driver initialization.
This is the main initialization function for the BMA180 device. The accelerometer range and bandwidth are set based on user-specified values from the system configuration.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
Bosch BMA220 accelerometer driver initialization.
This is the main initialization function for the BMA220 device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
Bosch BMA222 accelerometer driver initialization.
This is the main initialization function for the BMA222 device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
Bosch BMA250 accelerometer driver initialization.
This is the main initialization function for the BMA250 device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
Bosch BMP085 barometric sensor driver initialization.
This is the main initialization function for the BMP085 device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
Bosch BMP180 barometric sensor driver initialization.
This is the main initialization function for the BMP180 device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
Honeywell HMC5883L magnetometer driver initialization.
This is the main initialization function for the HMC5883L device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
References sensor_hal::bandwidth, sensor_map_t::bandwidth_Hz, sensor_hal::bus, data, DATA_RATE_15HZ, sensor_data_t::device, sensor_device_t::func, hmc5883l_calibrate(), HMC5883L_CONFIG_REG_A, HMC5883L_DATA_RESOLUTION, HMC5883L_DEV_ID, hmc5883l_device_id(), hmc5883l_ioctl(), HMC5883L_MODE_REG, hmc5883l_read(), hmc5883l_selftest(), hmc5883l_set_bandwidth(), hmc5883l_set_range(), index_130uT, index_15hz, MEAS_MODE_NORM, MODE_CONTIN, nvram_read(), cal_data_t::offsets, sensor_hal::range, sensor_map_t::range_units, sensor_funcs_t::read, sensor_hal::resolution, sensor_bus_put, SENSOR_CAPS_3_AXIS, SENSOR_CAPS_SELFTEST, SENSOR_SCALE_micro, SENSOR_UNITS_tesla, SENSOR_VENDOR_HONEYWELL, bus_desc_t::status, status, STATUS_OK, vector3_t::x, vector3_t::y, and vector3_t::z.
InvenSense IMU-3000 motion processor driver initialization.
This is the main initialization function for the IMU-3000 device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
InvenSense ITG-3200 gyroscope driver initialization.
This is the main initialization function for the ITG-3200 device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
Kionix KXTF9 accelerometer driver initialization.
This is the main initialization function for the KXTF9 device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
References ARRAYSIZE, band_table, sensor_hal::bandwidth, sensor_map_t::bandwidth_Hz, sensor_hal::burst_addr, sensor_hal::bus, CTRL_REG1_PC1, CTRL_REG1_RES, CTRL_REG3_OTDT_400HZ, CTRL_REG3_OTP_6_3HZ, CTRL_REG3_OWUF_50HZ, CTRL_REG3_SRST, DATA_CTRL_ODR_200HZ, delay_ms, sensor_device_t::func, INDEX_2G, INT_CTRL_REG1_IEA, INT_CTRL_REG1_IEL, INT_CTRL_REG1_IEN, KXTF9_CTRL_REG1, KXTF9_CTRL_REG3, KXTF9_DATA_CTRL_REG, KXTF9_DATA_RESOLUTION, kxtf9_event(), KXTF9_ID_VAL, KXTF9_INT_CTRL_REG1, KXTF9_INT_REL, kxtf9_ioctl(), kxtf9_isr(), kxtf9_read(), KXTF9_TILT_TIMER, KXTF9_WHO_AM_I, KXTF9_WUF_TIMER, KXTF9_XOUT_L, KXTI9_ID_VAL, sensor_hal::mcu_sigint, ODR_INDEX_50HZ, sensor_hal::range, range_table, sensor_map_t::range_units, sensor_funcs_t::read, RESET_DELAY_MSEC, sensor_hal::resolution, sensor_hal::sample_rate, sensor_bus_get, sensor_bus_put, SENSOR_CAPS_3_AXIS, SENSOR_CAPS_HI_G_EVENT, SENSOR_CAPS_LO_G_EVENT, SENSOR_CAPS_SELFTEST, SENSOR_CAPS_TAP_EVENT, SENSOR_CAPS_TILT_EVENT, sensor_irq_connect(), SENSOR_SCALE_milli, SENSOR_UNITS_g0, SENSOR_VENDOR_KIONIX, START_DELAY_MSEC, bus_desc_t::status, status, STATUS_OK, TILT_TIMER_INIT, and WUF_TIMER_INIT.
Osram SFH5712 light sensor driver initialization.
This is the main initialization function for the SFH5712 device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
Osram SFH7770 light & proximity sensor driver initialization.
This is the main initialization function for the SFH7770 device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |