Microchip® Advanced Software Framework

sensor_map_t Struct Reference

Sensor Operational Capabilities Descriptors.

#include <sensor.h>

Data Fields

union {
   int16_t   bandwidth_Hz
 Engineering unit value (Hz.) More...
 
   int16_t   range_units
 Engineering unit value (varies) More...
 
}; 
 
uint8_t reserved_val
 Driver-specific reserved value. More...
 

union { ... }
int16_t sensor_map_t::bandwidth_Hz
int16_t sensor_map_t::range_units

Engineering unit value (varies)

Referenced by hmc5883l_init(), kxtf9_init(), and sensor_range_index().

uint8_t sensor_map_t::reserved_val

Driver-specific reserved value.

Referenced by imu3000_default_init().