Physical Abstraction Layer.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
#include <string.h>
#include "asf.h"
#include "conf_pal.h"
Functions | |
static uint8_t | _pal_get_ex_snr (void) |
Get the extended signal noise ratio value. More... | |
static uint8_t | _pal_get_qt (void) |
Calculates the QT value with the last message rx parameters. More... | |
static void | pal_get_rx (void *pvParameters) |
Get result from reception. More... | |
static void | pal_get_tx_result (void *pvParameters) |
Get result from transmission. More... | |
void | pal_init (void) |
This function initiates PRIME PHY layer configuration and it must be implemented externally by the user. More... | |
void | pal_process (void) |
This function runs the PAL layer process. More... | |
void | pal_data_indication (uint8_t *puc_psdu, uint16_t *pus_len, uint8_t *puc_level, uint8_t *puc_scheme, uint32_t *pul_time) |
Check if a message has been received from PHY layer. More... | |
uint8_t | pal_data_request (uint8_t *puc_mpdu, uint16_t us_len, uint8_t uc_level, uint8_t uc_scheme, uint32_t ul_time) |
Send message using standard PHY layer. More... | |
uint8_t | pal_timer_get (uint32_t *pul_timer) |
Get timer. More... | |
uint8_t | pal_cd_get (uint8_t *puc_cd, uint8_t *puc_rssi, uint32_t *pul_time, uint8_t *puc_header) |
Get carrier detect. More... | |
uint8_t | pal_zct_get (uint32_t *pul_zct) |
Get zero-cross time. More... | |
uint8_t | pal_agc_get (uint8_t *puc_mode, uint8_t *puc_gain) |
Get Automatic Gain Mode (AGC) More... | |
uint8_t | pal_agc_set (uint8_t uc_mode, uint8_t uc_gain) |
Set Automatic Gain Mode (AGC) More... | |
uint8_t | pal_nl_get (uint8_t *puc_noise) |
Get Noise Level (NL) More... | |
uint8_t | pal_snr_get (uint8_t *puc_snr, uint8_t uc_qt) |
Get Signal Noise Ratio (SNR) More... | |
void | pal_data_indication_ex (xPalMsgRx_t *px_msg) |
Check if a message has been received from PHY layer. More... | |
uint8_t | pal_data_request_ex (xPalMsgTx_t *px_msg) |
Send message using PHY layer. More... | |
uint8_t | pal_get_cfg_ex (uint16_t us_id, void *p_val, uint16_t uc_len) |
Get extended PHY layer parameter. More... | |
uint8_t | pal_set_cfg_ex (uint16_t us_id, void *p_val, uint16_t uc_len) |
Set extended PHY layer parameter. More... | |
uint8_t | pal_cmd_cfg_ex (uint16_t us_id, uint8_t uc_cmd, uint8_t uc_mask) |
Binary Command extended PHY layer parameter. More... | |
Variables | |
uint32_t | l_tx_time |
const uint32_t | phyEvmThresholdEx [] |
static uint8_t | uc_pal_crc_enable |
static uint8_t | uc_pal_data_buf_rx [PHY_MAX_PPDU_SIZE] |
static uint8_t | uc_rx_msg_flag |
static uint8_t | uc_tx_bcn_res_flag |
uint8_t | uc_tx_delay |
uint8_t | uc_tx_head_type |
uint8_t | uc_tx_level |
static uint8_t | uc_tx_res_flag |
uint8_t | uc_tx_scheme |
static uint16_t | ul_rx_bad_crc |
static uint16_t | ul_rx_false_positive |
static xPhyMsgTxResult_t | x_pal_bcn_tx_res |
static xPhyMsgRx_t | x_pal_rx_msg |
static xPhyMsgTxResult_t | x_pal_tx_res |