Network interface and stateless autoconfiguration (RFC 4862)
#include "net/ip/uip.h"
#include "sys/stimer.h"
#include "net/ipv6/uip-nd6.h"
#include "net/ipv6/uip-ds6-route.h"
#include "net/ipv6/uip-ds6-nbr.h"
#include "compiler.h"
Data Structures | |
struct | uip_ds6_aaddr |
Anycast address. More... | |
struct | uip_ds6_addr |
Unicast address structure. More... | |
struct | uip_ds6_element |
Generic type for a DS6, to use a common loop though all DS. More... | |
struct | uip_ds6_maddr |
A multicast address. More... | |
struct | uip_ds6_netif |
Interface structure (contains all the interface variables) More... | |
struct | uip_ds6_prefix |
A prefix list entry. More... | |
Typedefs | |
typedef struct uip_ds6_aaddr | uip_ds6_aaddr_t |
Anycast address. More... | |
typedef struct uip_ds6_addr | uip_ds6_addr_t |
Unicast address structure. More... | |
typedef struct uip_ds6_element | uip_ds6_element_t |
Generic type for a DS6, to use a common loop though all DS. More... | |
typedef struct uip_ds6_maddr | uip_ds6_maddr_t |
A multicast address. More... | |
typedef struct uip_ds6_netif | uip_ds6_netif_t |
Interface structure (contains all the interface variables) More... | |
typedef struct uip_ds6_prefix | uip_ds6_prefix_t |
A prefix list entry. More... | |
Functions | |
uint8_t | get_match_length (uip_ipaddr_t *src, uip_ipaddr_t *dst) |
Get the number of matching bits of two addresses. More... | |
uint32_t | uip_ds6_compute_reachable_time (void) |
Compute the reachable time based on base reachable time, see RFC 4861. More... | |
void | uip_ds6_init (void) |
Initialize data structures. More... | |
uint8_t | uip_ds6_list_loop (uip_ds6_element_t *list, uint8_t size, uint16_t elementsize, uip_ipaddr_t *ipaddr, uint8_t ipaddrlen, uip_ds6_element_t **out_element) |
Generic loop routine on an abstract data structure, which generalizes all data structures used in DS6. More... | |
void | uip_ds6_periodic (void) |
Periodic processing of data structures. More... | |
void | uip_ds6_select_src (uip_ipaddr_t *src, uip_ipaddr_t *dst) |
Source address selection, see RFC 3484. More... | |
void | uip_ds6_send_ra_periodic (void) |
Send a periodic RA. More... | |
void | uip_ds6_send_ra_sollicited (void) |
Send a RA as an asnwer to a RS. More... | |
void | uip_ds6_set_addr_iid (uip_ipaddr_t *ipaddr, uip_lladdr_t *lladdr) |
set the last 64 bits of an IP address based on the MAC address More... | |
Prefix list basic routines | |
uip_ds6_prefix_t * | uip_ds6_prefix_add (uip_ipaddr_t *ipaddr, uint8_t length, uint8_t advertise, uint8_t flags, unsigned long vtime, unsigned long ptime) |
void | uip_ds6_prefix_rm (uip_ds6_prefix_t *prefix) |
uip_ds6_prefix_t * | uip_ds6_prefix_lookup (uip_ipaddr_t *ipaddr, uint8_t ipaddrlen) |
uint8_t | uip_ds6_is_addr_onlink (uip_ipaddr_t *ipaddr) |
Unicast address list basic routines | |
uip_ds6_addr_t * | uip_ds6_addr_add (uip_ipaddr_t *ipaddr, unsigned long vlifetime, uint8_t type) |
void | uip_ds6_addr_rm (uip_ds6_addr_t *addr) |
uip_ds6_addr_t * | uip_ds6_addr_lookup (uip_ipaddr_t *ipaddr) |
uip_ds6_addr_t * | uip_ds6_get_link_local (int8_t state) |
uip_ds6_addr_t * | uip_ds6_get_global (int8_t state) |
Multicast address list basic routines | |
uip_ds6_maddr_t * | uip_ds6_maddr_add (const uip_ipaddr_t *ipaddr) |
void | uip_ds6_maddr_rm (uip_ds6_maddr_t *maddr) |
uip_ds6_maddr_t * | uip_ds6_maddr_lookup (const uip_ipaddr_t *ipaddr) |
Anycast address list basic routines | |
uip_ds6_aaddr_t * | uip_ds6_aaddr_add (uip_ipaddr_t *ipaddr) |
void | uip_ds6_aaddr_rm (uip_ds6_aaddr_t *aaddr) |
uip_ds6_aaddr_t * | uip_ds6_aaddr_lookup (uip_ipaddr_t *ipaddr) |
Variables | |
uip_ds6_netif_t | uip_ds6_if |
uip_ds6_prefix_t | uip_ds6_prefix_list [UIP_DS6_PREFIX_NB] |
The single interface. More... | |
struct etimer | uip_ds6_timer_periodic |
#define uip_ds6_is_my_aaddr | ( | addr | ) | (uip_ds6_aaddr_lookup(addr) != NULL) |
#define uip_ds6_is_my_addr | ( | addr | ) | (uip_ds6_addr_lookup(addr) != NULL) |
Referenced by ns_input(), resolv_found(), tcpip_ipv6_output(), uip_nd6_ns_output(), and uip_process().
#define uip_ds6_is_my_maddr | ( | addr | ) | (uip_ds6_maddr_lookup(addr) != NULL) |
Referenced by uip_process().