Microchip® Advanced Software Framework

sha204_example_led.c File Reference
#include <stdio.h>
#include "asf.h"
#include "compiler.h"
#include "preprocessor.h"
#include "led.h"
#include "sha204_example_led.h"
#include "sha204_timer.h"

Functions

void display_status (uint8_t device_present_mask, uint8_t sha204_revision)
 This function displays information using LEDs about the SHA204 devices on the Security Xplained board. More...
 
void led_display_number (uint8_t value)
 This function displays a byte value using the Xplained LEDs. More...