|
void | QDebug_Init (void) |
| Initialize Debug InterfaceMust be called before the main loop. More...
|
|
void | QDebug_ProcessCommands (void) |
| Command handler for the data received from QTouch StudioThis function should be called in the main loop after measure_sensors to process the data received from QTOuch Studio More...
|
|
void | QDebug_SendData (uint16_t qt_lib_flags) |
| Send data to QTouch Studio based on the subscriptionThis function should be called in the main loop after measure_sensors to send the measured touch data. More...
|
|
void | QDebug_SetSubscriptions (uint16_t once, uint16_t change, uint16_t allways) |
| Set subscription values. More...
|
|
void | Set_Channel_Config (void) |
| Extract the data packet from QTouch Studio and set channel configShould only be called from the command handler. More...
|
|
void | Set_Global_Config (void) |
| Extract the data packet from QTouch Studio and set global configShould only be called from the command handler. More...
|
|
void | Set_QM_Burst_Lengths (void) |
| Set QMatrix burst lengthsShould only be called from the command handler. More...
|
|
void | Set_QT_User_Data (uint8_t *pdata) |
| Extracts user data from QTouch Studio to touch mcu memoryThe data can be binary data. More...
|
|
void | Set_Subscriptions (void) |
| Set Data Subscription valuesShould only be called from the command handler. More...
|
|
void | Transmit_Burst_Lengths (void) |
| Transmits the QMatrix burst length values to QTouch StudioThis value is available for each channel. More...
|
|
void | Transmit_Delta (void) |
| Transmits the channel delta values to QTouch StudioThe value is equal to signal-reference. More...
|
|
void | Transmit_Dummy (void) |
| Transmits a dummy packet if no other subscriptions are set. More...
|
|
void | Transmit_Global_Config (void) |
| Transmits the global config struct to QTouch Studio. More...
|
|
void | Transmit_QT_User_Data (uint8_t *pdata, uint16_t c) |
| Transmits user data to QTouch StudioThe data will be binary data. More...
|
|
void | Transmit_Ref (void) |
| Transmits the channel reference values to QTouch Studio. More...
|
|
void | Transmit_Sensor_Config (void) |
| Transmits the channel config struct to QTouch Studio. More...
|
|
void | Transmit_Sign_On (void) |
| Transmits the sign on packet to QTouch Studio. More...
|
|
void | Transmit_Signals (void) |
| Transmits the measurement values for each channel to QTouch Studio. More...
|
|
void | Transmit_State (void) |
| Transmits the state values to QTouch StudioOn/Off condition for each sensor. More...
|
|
void | Transmit_Time_Stamps (void) |
| Transmits the application execution timestamp values to QTouch StudioThis value is a combination of current_time_ms_touch (high word) & timer counter register (low word) More...
|
|