Bosch BMA220 3-axis accelerometer driver.
This file contains functions for initializing and reading data from a Bosch BMA220 3-axis accelerometer.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | REG_ADDR(reg) ((reg) * burst_increment) |
Functions | |
static bool | bma220_device_id (sensor_hal_t *hal, sensor_data_t *data) |
Read BMA220 device ID and revision numbers. More... | |
static bool | bma220_event (sensor_t *sensor, sensor_event_t sensor_event, sensor_event_callback_t *callback, bool enable) |
Enable or disable BMA220 sensor events. More... | |
static bool | bma220_get_accel (sensor_hal_t *hal, sensor_data_t *data) |
Read BMA220 acceleration data. More... | |
static bool | bma220_get_threshold (sensor_hal_t *hal, sensor_threshold_desc_t *threshold) |
Get a BMA220 event threshold value. More... | |
bool | bma220_init (sensor_t *sensor, int resvd) |
Bosch BMA220 accelerometer driver initialization. More... | |
static bool | bma220_ioctl (sensor_t *sensor, sensor_command_t cmd, void *arg) |
BMA220 ioctl control entry point. More... | |
static void | bma220_isr (volatile void *arg) |
Bosch BMA220 driver interrupt service routine. More... | |
static bool | bma220_read (sensor_t *sensor, sensor_read_t type, sensor_data_t *data) |
Read sensor data. More... | |
static bool | bma220_selftest (sensor_t *sensor, int *test_code, void *arg) |
Run BMA220 self-tests. More... | |
static bool | bma220_set_bandwidth (sensor_hal_t *hal, int16_t band) |
Set the BMA220 digital filter cut-off frequency. More... | |
static bool | bma220_set_range (sensor_hal_t *hal, int16_t range) |
Set the BMA220 full scale acceleration range. More... | |
static bool | bma220_set_state (sensor_t *sensor, sensor_state_t mode) |
Set the BMA220 execution mode. More... | |
static bool | bma220_set_tap (sensor_hal_t *hal, sensor_tap_params_t *params) |
Set up tap detection parameters. More... | |
static bool | bma220_set_threshold (sensor_hal_t *hal, sensor_threshold_desc_t *threshold) |
Set a BMA220 event threshold value. More... | |
static void | bma220_sleep_en (sensor_hal_t *hal, bool sleep) |
Enable or disable the BMA220 sleep mode. More... | |
Variables | |
static const sensor_map_t | band_table [] |
Bosch BMA220 Bandwidth Table (hertz, register value) More... | |
static uint8_t | burst_increment |
Burst Address Adjustment. More... | |
static sensor_event_callback_t | event_cb [5] |
Sensor Event Callback Descriptors (data=0, motion=1, low-g=2, high-g=3, tap=4) More... | |
struct { | |
union { | |
uint8_t status_byte [2] | |
Status bytes. More... | |
struct { | |
uint8_t data_int: 1 | |
New data interrupt triggered. More... | |
uint8_t high_int: 1 | |
High-g criteria triggered. More... | |
uint8_t int_first_x: 1 | |
x-axis triggered any-motion interrupt More... | |
uint8_t int_first_y: 1 | |
y-axis triggered any-motion interrupt More... | |
uint8_t int_first_z: 1 | |
z-axis triggered any-motion interrupt More... | |
uint8_t int_sign: 1 | |
Axis motion direction. More... | |
uint8_t low_int: 1 | |
Low-g criteria triggered. More... | |
uint8_t orient: 3 | |
Orientation with respect to gravity. More... | |
uint8_t orient_int: 1 | |
< Status fields More... | |
uint8_t slope_int: 1 | |
Slope criteria triggered. More... | |
uint8_t tt_int: 1 | |
Tap criteria triggered. More... | |
uint8_t unused: 3 | |
} status_field | |
} | |
bma_axis_t acc [3] | |
Acceleration data. More... | |
uint8_t unused [6] | |
Unused register space. More... | |
} | event_regs |
Sensor Event Registers. More... | |
static const sensor_map_t | range_table [] |
Bosch BMA220 Range Table (milli-g, register value) More... | |
#define REG_ADDR | ( | reg | ) | ((reg) * burst_increment) |
|
static |
Read BMA220 device ID and revision numbers.
This function reads the accelerometer hardware identification registers and returns these values in the specified data structure.
hal | Address of an initialized sensor hardware descriptor. |
data | Address of sensor_data_t structure to return values. |
References BMA220_CHIP_ID, BMA220_CHIP_VERSION, sensor_data_t::device, REG_ADDR, and sensor_bus_get.
Referenced by bma220_read().
|
static |
Enable or disable BMA220 sensor events.
sensor | Address of an initialized sensor device descriptor |
sensor_event | Specifies the sensor event type |
callback | Application-defined event callback handler descriptor |
enable | Enable flag: true = enable event, false = disable event |
References BMA220_INT_ENABLE1, BMA220_INT_ENABLE2, EN_DATA_FIELD, EN_HIGH_X_FIELD, EN_HIGH_Y_FIELD, EN_HIGH_Z_FIELD, EN_LOW_FIELD, EN_SLOPE_X_FIELD, EN_SLOPE_Y_FIELD, EN_SLOPE_Z_FIELD, EN_TT_X_FIELD, EN_TT_Y_FIELD, EN_TT_Z_FIELD, sensor_desc::hal, LATCH_INT_FIELD, REG_ADDR, RESET_INT, sensor_bus_get, sensor_bus_put, SENSOR_EVENT_HIGH_G, SENSOR_EVENT_LOW_G, SENSOR_EVENT_MOTION, SENSOR_EVENT_NEW_DATA, SENSOR_EVENT_TAP, and status.
Referenced by bma220_init(), and bma220_ioctl().
|
static |
Read BMA220 acceleration data.
This function obtains accelerometer data for all three axes of the Bosch device. The data is read from three device registers using a multi-byte bus transfer.
Along with the actual sensor data, the LSB byte contains a "new" flag indicating if the data for this axis has been updated since the last time the axis data was read. Reading either LSB or MSB data will clear this flag.
sensor | Address of an initialized sensor device descriptor. |
data | The address of a vector storing sensor axis data. |
References sensor_hal::burst_addr, event_regs, and sensor_bus_read.
Referenced by bma220_ioctl(), and bma220_read().
|
static |
Get a BMA220 event threshold value.
hal | Address of an initialized sensor hardware descriptor. |
threshold | Address of threshold descriptor. |
References BMA220_HG_LG_THRESHOLD, BMA220_SLOPE_CONFIG, sensor_hal::range, REG_ADDR, sensor_bus_get, SENSOR_THRESHOLD_HIGH_G, SENSOR_THRESHOLD_LOW_G, SENSOR_THRESHOLD_MOTION, SENSOR_THRESHOLD_TAP, SENSOR_THRESHOLD_TILT, sensor_threshold_desc_t::type, and sensor_threshold_desc_t::value.
Referenced by bma220_ioctl().
Bosch BMA220 accelerometer driver initialization.
This is the main initialization function for the BMA220 device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
References ARRAYSIZE, band_table, sensor_hal::bandwidth, BMA220_CHIP_ID, BMA220_DATA_RESOLUTION, bma220_event(), BMA220_ID_VAL, bma220_ioctl(), bma220_isr(), bma220_read(), bma220_selftest(), bma220_set_state(), BMA220_X_AXIS_DATA, sensor_hal::burst_addr, burst_increment, sensor_hal::bus, BUS_TYPE_TWI, sensor_desc::drv, sensor_device_t::func, sensor_desc::hal, sensor_hal::mcu_sigint, sensor_hal::range, range_table, sensor_funcs_t::read, REG_ADDR, sensor_hal::resolution, sensor_bus_get, SENSOR_CAPS_3_AXIS, SENSOR_CAPS_HI_G_EVENT, SENSOR_CAPS_LO_G_EVENT, SENSOR_CAPS_SELFTEST, SENSOR_CAPS_TAP_EVENT, SENSOR_CAPS_TILT_EVENT, sensor_irq_connect(), SENSOR_SCALE_milli, SENSOR_STATE_RESET, SENSOR_UNITS_g0, SENSOR_VENDOR_BOSCH, status, bus_desc_t::status, STATUS_OK, and bus_desc_t::type.
|
static |
BMA220 ioctl control entry point.
hal | Address of an initialized sensor hardware descriptor. |
cmd | Command to execute |
arg | Argument for command (varies) |
References sensor_data_t::axis, bma220_event(), bma220_get_accel(), bma220_get_threshold(), bma220_set_bandwidth(), bma220_set_range(), bma220_set_state(), bma220_set_tap(), bma220_set_threshold(), sensor_desc::err, sensor_desc::hal, sensor_desc::mod, sensor_data_t::scaled, SENSOR_DISABLE_EVENT, SENSOR_ENABLE_EVENT, SENSOR_ERR_UNSUPPORTED, SENSOR_GET_THRESHOLD, SENSOR_READ_VECTOR, SENSOR_SET_BANDWIDTH, SENSOR_SET_RANGE, SENSOR_SET_STATE, SENSOR_SET_TAP, SENSOR_SET_THRESHOLD, SENSOR_STATE_NORMAL, SENSOR_STATE_RESET, vector3_t::x, vector3_t::y, and vector3_t::z.
Referenced by bma220_init().
|
static |
Bosch BMA220 driver interrupt service routine.
This is the common interrupt service routine for all enabled BMA220 interrupt events. Five different types of interrupts can be programmed. All interrupt criteria are combined and drive the interrupt pad with a Boolean OR
condition.
Interrupt criteria are tested against values from the BMA220 digital filter output. All thresholds are scaled using the current device range. Timings for high and low acceleration are absolute values (1 LSB of HG_dur and LG_dur registers corresponds to 1 millisecond, +/- 10%). Timing for the any-motion interrupt and alert detection are proportional to the bandwidth setting.
This routine handles interrupts generated when low-g, high-g, any-motion, alert, and new data criteria are satisfied and the corresponding event notification is enabled in the device.
The BMA220 device does not provide any way to definitively identify an any-motion interrupt once it has occurred. So, if a handler has been installed for that event, it will always be called by this routine, and the SENSOR_EVENT_MOTION indicator will be set in the event type field.
arg | The address of the driver sensor_hal_t descriptor. |
References sensor_hal::burst_addr, sensor_hal::bus, sensor_event_data_t::data, sensor_event_data_t::event, event_regs, sensor_event_callback_t::handler, bus_desc_t::no_wait, sensor_data_t::scaled, sensor_bus_read, SENSOR_EVENT_HIGH_G, SENSOR_EVENT_LOW_G, SENSOR_EVENT_MOTION, SENSOR_EVENT_NEW_DATA, SENSOR_EVENT_TAP, SENSOR_EVENT_UNKNOWN, sensor_timestamp(), bus_desc_t::status, STATUS_OK, and sensor_data_t::timestamp.
Referenced by bma220_init().
|
static |
Read sensor data.
This routine calls the appropriate internal data function to obtain the specified type of data from the sensor device.
sensor | Address of an initialized sensor device descriptor. |
type | Type of sensor data to read. |
data | The address where data values are returned. |
References bma220_device_id(), bma220_get_accel(), sensor_desc::err, sensor_desc::hal, SENSOR_ERR_FUNCTION, SENSOR_READ_ACCELERATION, and SENSOR_READ_ID.
Referenced by bma220_init().
Run BMA220 self-tests.
sensor | Address of an initialized sensor device descriptor. |
test_code | Address of a device-specific numeric test code. |
arg | Device-specific self-test argument options. |
References SENSOR_TEST_DEFLECTION.
Referenced by bma220_init().
|
static |
Set the BMA220 digital filter cut-off frequency.
hal | Address of an initialized sensor hardware descriptor. |
band | The index of a driver-specific bandwidth table entry. |
References BMA220_BANDWIDTH_CONFIG, FILTER_CONFIG_FIELD, REG_ADDR, and sensor_reg_fieldset.
Referenced by bma220_ioctl().
|
static |
Set the BMA220 full scale acceleration range.
hal | Address of an initialized sensor hardware descriptor. |
range | The index of a driver-specific range table entry. |
References BMA220_RANGE_SELFTEST, RANGE_FIELD, REG_ADDR, and sensor_reg_fieldset.
Referenced by bma220_ioctl().
|
static |
Set the BMA220 execution mode.
This routine sets a specified BMA220 execution state to one of the following:
SENSOR_STATE_SUSPEND or SENSOR_STATE_LOWEST_POWER The BMA220 can be put into a suspend mode to easily achieve a power consumption below 1uA. In this mode all analog modules except for power-on reset will be disabled. Only reads through the serial interface are supported during suspend.
SENSOR_STATE_SLEEP or SENSOR_STATE_LOW_POWER This option sets the BMA220 to a low-power mode. In this mode, the device periodically wakes up, evaluates acceleration data with respect to interrupt criteria defined by the user and goes back to sleep if no interrupt has occurred using the following procedure:
SENSOR_STATE_NORMAL or SENSOR_STATE_HIGHEST_POWER In normal mode the sensor IC data and status registers can be accessed without restriction. The device current consumption is typically 250 microamps in this state.
SENSOR_STATE_X_AXIS_STANDBY SENSOR_STATE_Y_AXIS_STANDBY SENSOR_STATE_Z_AXIS_STANDBY In order to optimize further power consumption of the BMA220, data evaluation of individual axes can be deactivated.
SENSOR_STATE_RESET This function resets the device and internal registers to the power-up default settings.
sensor | Address of a sensor device descriptor. |
mode | A specified sensor operational mode. |
References bma220_sleep_en(), BMA220_SOFTRESET, BMA220_SUSPEND_MODE, sensor_desc::hal, sensor_desc::mod, REG_ADDR, sensor_bus_get, SENSOR_STATE_HIGHEST_POWER, SENSOR_STATE_LOW_POWER, SENSOR_STATE_LOWEST_POWER, SENSOR_STATE_NORMAL, SENSOR_STATE_RESET, SENSOR_STATE_SLEEP, and SENSOR_STATE_SUSPEND.
Referenced by bma220_init(), and bma220_ioctl().
|
static |
Set up tap detection parameters.
hal | Address of an initialized sensor hardware descriptor. |
params | Address of an initialized tap parameter structure. |
Referenced by bma220_ioctl().
|
static |
Set a BMA220 event threshold value.
hal | Address of an initialized sensor hardware descriptor. |
threshold | Address of threshold descriptor. |
References BMA220_HG_LG_THRESHOLD, BMA220_SLOPE_CONFIG, BMA220_TAP_CONFIG, HIGH_TH_FIELD, LOW_TH_FIELD, sensor_hal::range, REG_ADDR, sensor_reg_fieldset, SENSOR_THRESHOLD_HIGH_G, SENSOR_THRESHOLD_LOW_G, SENSOR_THRESHOLD_MOTION, SENSOR_THRESHOLD_TAP, SENSOR_THRESHOLD_TILT, SLOPE_TH_FIELD, THRESHOLD_IN_G, TT_TH_FIELD, sensor_threshold_desc_t::type, and sensor_threshold_desc_t::value.
Referenced by bma220_ioctl().
|
inlinestatic |
Enable or disable the BMA220 sleep mode.
This routine enables or disables the BMA220 sleep mode depending upon the value of the parameter; a value enables sleep mode and a value disables sleep mode by setting or clearing the 'sleep_en' bit, respectively.
hal | Address of an initialized sensor hardware descriptor. |
sleep | Set flag to enable sleep mode. |
References BMA220_SLEEP_CONFIG, sensor_reg_bitclear, sensor_reg_bitset, and SLEEP_ENABLE.
Referenced by bma220_set_state().
bma_axis_t acc[3] |
Acceleration data.
Referenced by sample_callback().
|
static |
Bosch BMA220 Bandwidth Table (hertz, register value)
Referenced by bma220_init().
|
static |
Burst Address Adjustment.
From SPI -> TWI use burst address increment in 2h steps.
Referenced by bma220_init().
uint8_t data_int |
New data interrupt triggered.
|
static |
Sensor Event Callback Descriptors (data=0, motion=1, low-g=2, high-g=3, tap=4)
struct { ... } event_regs |
Sensor Event Registers.
Referenced by bma220_get_accel(), and bma220_isr().
uint8_t high_int |
High-g criteria triggered.
uint8_t int_first_x |
x-axis triggered any-motion interrupt
uint8_t int_first_y |
y-axis triggered any-motion interrupt
uint8_t int_first_z |
z-axis triggered any-motion interrupt
uint8_t int_sign |
Axis motion direction.
uint8_t low_int |
Low-g criteria triggered.
uint8_t orient |
Orientation with respect to gravity.
Referenced by hmc5883l_get_data().
uint8_t orient_int |
< Status fields
Orientation interrupt triggered
|
static |
Bosch BMA220 Range Table (milli-g, register value)
Referenced by bma220_init().
uint8_t slope_int |
Slope criteria triggered.
uint8_t status_byte[2] |
Status bytes.
Referenced by sha204c_send_and_receive().
struct { ... } status_field |
uint8_t tt_int |
Tap criteria triggered.
uint8_t unused |
Unused register space.