Microchip® Advanced Software Framework

sha204_example_comm.c File Reference
#include <stdint.h>
#include <string.h>
#include "compiler.h"
#include "preprocessor.h"
#include "board.h"
#include "sysclk.h"
#include "sha204_example_led.h"
#include "sha204_timer.h"
#include "sha204_command_marshaling.h"
#include "sha204_lib_return_codes.h"
#include "security_xplained.h"

Functions

int main (void)
 This function is the entry function for an example application that uses the SHA204 ASF component. More...