This file contains the AT32UC3L QTouch Libary API interface for QMatrix, QTouch and Autonomous Touch method using the Capacitive Touch (CAT) module.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include <stdint.h>
#include <stdbool.h>
#include <stdlib.h>
#include "touch_config_at32uc3l.h"
Data Structures | |
struct | tag_sensor_t |
struct | tag_touch_at_config_t |
struct | tag_touch_at_param_t |
struct | tag_touch_at_pin_t |
struct | tag_touch_at_reg_t |
struct | tag_touch_at_status_t |
struct | tag_touch_config_t |
struct | tag_touch_filter_data_t |
struct | tag_touch_general_config_t |
struct | tag_touch_global_param_t |
struct | tag_touch_info_t |
struct | tag_touch_measure_data_t |
struct | tag_touch_qm_config_t |
struct | tag_touch_qm_dma_t |
struct | tag_touch_qm_param_t |
struct | tag_touch_qm_pin_t |
struct | tag_touch_qm_reg_t |
struct | tag_touch_qt_config_t |
struct | tag_touch_qt_param_t |
struct | tag_touch_qt_pin_t |
struct | tag_touch_qt_reg_t |
Macros | |
#define | PRIV_QT_RS_TABLE_INIT NULL |
Initialize rotor slider table. More... | |
QTouch Library Acquisition Status bitfields. | |
Enable QDebug interface | |
#define | TOUCH_NO_ACTIVITY (0x0000u) |
#define | TOUCH_IN_DETECT (0x0001u) |
#define | TOUCH_STATUS_CHANGE (0x0002u) |
#define | TOUCH_ROTOR_SLIDER_POS_CHANGE (0x0004u) |
#define | TOUCH_CHANNEL_REF_CHANGE (0x0008u) |
#define | TOUCH_BURST_AGAIN (0x0100u) |
#define | TOUCH_RESOLVE_CAL (0x0200u) |
#define | TOUCH_RESOLVE_FILTERIN (0x0400u) |
#define | TOUCH_RESOLVE_DI (0x0800u) |
#define | TOUCH_RESOLVE_POS_RECAL (0x1000u) |
QTouch method Acquisition Sensor Groups. | |
#define | TOUCH_QT_GRP_A (0u) |
#define | TOUCH_QT_GRP_B (1u) |
Functions | |
Autonomous QTouch API. | |
touch_ret_t | touch_at_sensor_init (touch_config_t *p_touch_config) |
This API is used to initialize the Touch Library with Autonomous Touch pin and register configuration provided by the user. More... | |
touch_ret_t | touch_at_sensor_update_config (touch_at_param_t *p_at_param) |
This API is used to update the register configuration information of the Autonomous Touch sensor. More... | |
touch_ret_t | touch_at_sensor_get_config (touch_at_param_t *p_at_param) |
This API is used to read back the register configuration information of the Autonomous Touch sensor. More... | |
touch_ret_t | touch_at_sensor_enable (void(*touch_at_status_change_interrupt_callback)(touch_at_status *p_at_status)) |
Enable the Autonomous Touch sensor to start Touch measurement. More... | |
touch_ret_t | touch_at_sensor_disable (void) |
Stop the Autonomous Touch sensor from doing Touch measurement. More... | |
touch_ret_t | touch_at_get_libinfo (touch_info_t *p_touch_info) |
This API can be used to read back Autonomous Touch configuration and status information in addition to the Touch Library version. More... | |
Common API. | |
void | touch_event_dispatcher (void) |
Touch Library Event Dispatcher. Common to QTouch Group A, QTouch Group B or QMatrix Acquisition methods. More... | |
void | touch_deinit (void) |
This API can be used to deinitialize the touch library. Once this API is called, both the QMatrix method and Autonomous Touch method acquisition is stopped and the CAT hardware module is disabled. More... | |
QTouch Library internal use functions. | |
void | touch_qm_rs_table_init (void) |
This Touch Library ISR must be registered to the Interrupt Controller module when using the GCC Compiler. More... | |
void | touch_qt_rs_table_init (void) |
This is an extern function of the Touch Library. This function is NOT to be used by the user. More... | |
void | touch_qta_table_init (void) |
This is an extern function of the Touch Library. This function is NOT to be used by the user. More... | |
void | touch_qtb_table_init (void) |
This is an extern function of the Touch Library. This function is NOT to be used by the user. More... | |
QMatrix API. | |
#define | touch_qm_sensors_init(x) |
touch_ret_t touch_qm_sensors_init( touch_config_t *p_touch_config); More... | |
touch_ret_t | touch_qm_sensors_init_with_rs_table (touch_config_t *p_touch_config,(void)) |
This API is used to initialize the Touch Library with QMatrix pin, register and sensor configuration provided by the user. More... | |
touch_ret_t | touch_qm_sensor_config (sensor_type_t sensor_type, channel_t from_channel, channel_t to_channel, aks_group_t aks_group, threshold_t detect_threshold, hysteresis_t detect_hysteresis, resolution_t position_resolution, uint8_t position_hysteresis, sensor_id_t *p_sensor_id) |
This API can be used to configure a sensor of type key, rotor or slider. More... | |
touch_ret_t | touch_qm_sensor_update_config (sensor_id_t sensor_id, touch_qm_param_t *p_touch_sensor_param) |
This API can be used to set the sensor configuration parameters. More... | |
touch_ret_t | touch_qm_sensor_get_config (sensor_id_t sensor_id, touch_qm_param_t *p_touch_sensor_param) |
This API can be used to read back the sensor configuration parameters information is being seeked. More... | |
touch_ret_t | touch_qm_channel_update_burstlen (channel_t channel_id, touch_bl_t qm_burst_length) |
This API can be used to update the burst length of a give input channel. More... | |
touch_ret_t | touch_qm_update_global_param (touch_global_param_t *p_global_param) |
This API can be used to update the global parameter of QMatrix method. More... | |
touch_ret_t | touch_qm_get_global_param (touch_global_param_t *p_global_param) |
This API can be used to read back the global parameter of QMatrix method. More... | |
touch_ret_t | touch_qm_sensors_calibrate (void) |
This API is used to calibrate the sensors for the first time before starting a Touch measurement. This API can also be used to force calibration of sensors when any of the Touch sensor parameters are changed during runtime. More... | |
touch_ret_t | touch_qm_sensors_start_acquisition (touch_time_t current_time_ms, touch_qm_dma_t *p_qm_dma, touch_acq_mode_t qm_acq_mode, void(*measure_complete_callback)(touch_measure_data_t *p_measure_data)) |
This API can be used to start a QMatrix Touch measurement. More... | |
touch_ret_t | touch_qm_get_libinfo (touch_info_t *p_touch_info) |
This API can be used to get the Touch Library configuration information for QMatrix Touch acquisition method. More... | |
touch_ret_t | touch_qm_sensor_get_delta (sensor_id_t sensor_id, touch_delta_t *p_delta) |
This API can be used retrieve the delta value corresponding to a given sensor. More... | |
QTouch Group A/Group B API. | |
#define | touch_qt_sensors_init(x, y) |
touch_ret_t touch_qt_sensors_init( touch_qt_grp_t touch_qt_grp, touch_config_t *p_touch_config); More... | |
touch_ret_t | touch_qt_sensors_init_with_rs_table (touch_qt_grp_t touch_qt_grp, touch_config_t *p_touch_config,(void),(void)) |
This API is used to initialize the Touch Library with QTouch Group A or QTouch Group B pin, register and sensor configuration provided by the user. More... | |
touch_ret_t | touch_qt_sensor_config (touch_qt_grp_t touch_qt_grp, sensor_type_t sensor_type, channel_t from_channel, channel_t to_channel, aks_group_t aks_group, threshold_t detect_threshold, hysteresis_t detect_hysteresis, resolution_t position_resolution, sensor_id_t *p_sensor_id) |
This API can be used to configure a sensor of type key, rotor or slider. More... | |
touch_ret_t | touch_qt_sensor_update_config (touch_qt_grp_t touch_qt_grp, sensor_id_t sensor_id, touch_qt_param_t *p_touch_sensor_param) |
This API can be used to set the sensor configuration parameters. More... | |
touch_ret_t | touch_qt_sensor_get_config (touch_qt_grp_t touch_qt_grp, sensor_id_t sensor_id, touch_qt_param_t *p_touch_sensor_param) |
This API can be used to read back the sensor configuration parameters. More... | |
touch_ret_t | touch_qt_update_global_param (touch_qt_grp_t touch_qt_grp, touch_global_param_t *p_global_param) |
This API can be used to update the global parameter of QTouch method. More... | |
touch_ret_t | touch_qt_get_global_param (touch_qt_grp_t touch_qt_grp, touch_global_param_t *p_global_param) |
This API can be used to read back the global parameter of QTouch method. More... | |
touch_ret_t | touch_qt_sensors_calibrate (touch_qt_grp_t touch_qt_grp) |
This API is used to calibrate the sensors for the first time before starting a Touch measurement. This API can also be used to force calibration of sensors when any of the Touch sensor parameters are changed during runtime. More... | |
touch_ret_t | touch_qt_sensors_start_acquisition (touch_qt_grp_t touch_qt_grp, touch_time_t current_time_ms, touch_qt_dma_t qt_dma_ch, touch_acq_mode_t qt_acq_mode, void(*measure_complete_callback)(touch_measure_data_t *p_measure_data)) |
This API can be used to start a QTouch Group A or QTouch Group B Touch measurement. More... | |
touch_ret_t | touch_qt_get_libinfo (touch_qt_grp_t touch_qt_grp, touch_info_t *p_touch_info) |
This API can be used to get the Touch Library configuration information for QTouch Group A or Group B acquisition method. More... | |
touch_ret_t | touch_qt_sensor_get_delta (touch_qt_grp_t touch_qt_grp, sensor_id_t sensor_id, touch_delta_t *p_delta) |
This API can be used retrieve the delta value corresponding to a given sensor. More... | |
touch_ret_t | touch_qt_sensor_disable (touch_qt_grp_t touch_qt_grp, sensor_id_t sensor_id) |
This API can be used disable acquisition on a given Touch Sensor. More... | |
touch_ret_t | touch_qt_sensor_reenable (touch_qt_grp_t touch_qt_grp, sensor_id_t sensor_id) |
This API can be used re-enable acquisition on a disabled Touch Sensor. More... | |